Greetings,
When debugging using CCS, it is not possible for me to step into functions provided by the qmss/cppi LLDs.
I've already tried the following attemps:
- Used "Debug" build configuration
- Set BIOS.libType = BIOS.LibType_Custom;
- Added the source-folders of the drivers to the debug-configuration: pdk_C6678_1_1_0_3\packages\ti\drv\qmss\src; pdk_C6678_1_1_0_3\packages\ti\drv\cppi\src
Yet all those attemps where unsucessul, and for now I had to manually include the source of both drivers in my project to get them built with debug-information - which works as expected.
Is there any trick to get cppi/qmms LLDs with debug-information without manually including the source in the project? Maybe something like BIOS.LibType_Custom, which forces a project-local recompilation using the project's settings?
Thx