Hello,
I have an ADS1298RECG-FE and would like to connect it to a DSP board for development purposes. hence, I need a board with an emulator and that is compatible with ADS1298.
I have seen the C5515-EVM and I have 2 questions:
1. Is it compatible with ADS1298RECG-FE REV.B? if it does, Which revision of the evm would be the most suitable?
2. Do you have a source code to start with in order to program the dsp? (For starter - I would like to create a small PC application).
Thank you very much,
Udi