Hello,
recently i've got this error:
C55xx: Error connecting to the target: Error 0x80000244/-1143 Fatal Error during: Register, Initialization, OCS, The memory at 0x00000000 continually indicated it was 'not ready' All memory operations currently in progress were aborted in order to regain control of the processor. This is considered a catastrophic event, but the debugger should still be able to access memory and CPU registers. System state has been altered. It is strongly advised that the processor should be reset before resuming execution,
I am workinng with EVM5515 and it was working fine but now i got this and I didn't do anything strange.
Please I would need some urgent help.
Best regards!