Other Parts Discussed in Thread: UCD9222
Hi
We are using a C6657CZH device. The core voltage is controlled by a UCD9222.
Control of the core voltage seems not to work. After PowerUp I see a low pulse on VCNTL3 (1.7ms long), after this all the VCNTL pins are stable high.
Is this the right behaviour? Is the VCNTL values presented only once after PU? If so, what is the timing related to RESET?
Otherwise, the chip is functioning OK, with core=1.1V
BR
Lars P