This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to enable both the Ethernet port in 6678

hi

  i am  using 6678 device which is having two Ethernet port in it. in my application i need to enable both of them but all example enable only one port.

how i can enable both using NDK or any other way.

pratik jain

  • Pratik,

    There are several forum threads discussing using a second port on a 6678, as well as other devices.  You can search the BIOS forum for “two Ethernet port” to find these.

    Two that should directly help are this one: http://e2e.ti.com/support/embedded/bios/f/355/t/244238.aspx

    And this one: http://e2e.ti.com/support/embedded/bios/f/355/t/260191.aspx

    Scott

  • scott

     i have tried as per  http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/196772.aspx  this link

     i am able to enable both ports but not able to set different IP add to them 

    my requirement is to use both ports as different network connection 

    please help me for this

    pratik jain

  • Pratik,

    Maybe this forum thread helps…  http://e2e.ti.com/support/embedded/bios/f/355/t/268788.aspx

    Scott