Other Parts Discussed in Thread: AM3352, TMDXEVM3358
Hello,
I have a trouble to boot from MMC1 (eMMC) on AM3352.
The eMMC is connected as defined in the TRM "Pins Used for MMC1 Boot" table, however the system can't be booted.
What case do you consider for this trouble?
(Already I checked "http://e2e.ti.com/support/arm/sitara_arm/f/791/p/196388/700616.aspx#700616")
Also, I tried to boot from MMC1 (eMMC) by using TMDXEVM3358.
The first trying conditions are following:
- using TMDXEVM3358 (REV 1.4A)
- using MMC1 port
- using included Linux SDK SD card (v5.04.01)
- PROFILE SELECTION (SW6) is all off (0000)
In above conditions, Linux is not booted.
Instead of setting SW6 to 0000, I only set switch=2 to 1 (switch-1234 = 0100).
Then, the boot is succeeded.
Why should I change the SW6 setting for booting?
If this change concerns to the MMC1 booting, should the eMMC connection be changed?
Best Regards
Nomoto