This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Platform inheritance in new platform wizard

Hello!

In my company we are developing custom board with C6670. It is different from EVM at least in having just single DDR3 memory chip. So to proceed with further development I guess I have to define my own platform package. I am using the most recent tools so far. These are CCS 5.4 and XDCtools 3.25.00.48. Demo provided in help refers to CCS 4, so my steps are somewhat different.

I invoke new platform wizard from File/New/Other menu. Then I follow steps in demo, give a name to the package, select folder, family and device itself.

At step 2 the demo suggest to import closest possible platform. The wizard offers me just single choice: ti.platforms.evm6614. As far as I can see from product folder, 6614 though shares many features of 6670 is quite different from it. So I'd rather import settings for 6670 evaluation module. However, as I mentioned, I have just singe option. Should I worry about that? Is there any method to refer evm6670 instead?