Hi,
I am confused by the power consumption on one of our C5505 based board. We have the board connected to PC with XDS100v2 USB emulator. The board is powered by a 3.7V power supply. The supply current normally is 115mA @ 3.7 V. However, if we add some 'asm(" nop");' into the code, the supply current will show 135mA @ 3.7V. Has anyone ever encounter this kind of symptom? CSL-3.3 and 2.5 both have the same symptom under CCSv5.4.
Thanks,
Jack