Hello
We're using a C6748 DSP and are interested in the different sleep modes.
We've seen that the following modes exist:
- C674x DSP CPU Sleep Mode => The DSP CPU can be put in a low-power state by executing the IDLE instruction.
- C674x Megamodule Sleep Mode => shut down the entire C674x megamodule
- RTC-Only Sleep Mode => only the RTC is powered on and the rest of the device is completely powered off
- Deep Sleep Mode => all device clocks are stopped and the on-chip oscillator is shut down to save power.
What is the wakeup delay for each of these modes?
We didn't find information on this in the Technical Reference Manual.
Thank you!
Best regards
Nicolas