Hello,
I'm working with a beagleboard. I’m booting an image via network using TFTP protocol, but after run bootm command it stops in “Uncompressing Linux...done”, booting the kernel”. These are my steps:
1) Stop autoboot
2) Configure values
- setenv ipaddr 192.168.10.10
- setenv serverip 192.168.10.20
- setenv netmaskip 255.255.255.0
- setenv gatewayip 192.168.10.1
3) check console value
- printenv console
- console=ttyO2,115200n8
4) dcache off
5) usb start
6) load image
- tftpboot /tftpboot/uImage
7) bootm
“Uncompressing Linux...done”, booting the kernel”
Autobooting the same file from mmc works.
What is it wrong? Whan can I do?
Thanks.