This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Dummy cycles requirement in Quad read mode of N25Q032A SPI flash

Hello Friends,

I have N25Q032 flash connected to TI DSP. I have a questions related to requirement of dummy cycles with respect to different opcodes modes of N25Q032 flash. 
I wanted to communicate with it at 100MHz with less overhead. Therefore I will be using Quad mode of operation (command, address and data on all four lines) i.e. Quad SPI Protocol.
Looking at table-13 'Supported clock frequencies':
If I use Quad I/O FAST read (0xEB) mode, then I need to use 9 dummy cycles.
But If I use FAST Read (0x0B) mode, then looks like I may need only 3 dummy cycles.
So, my question is if the protocol in both modes is same (command, ADDR and data on DQ[3:0]), why there is difference in dummy cycles when using these two modes? How SPI behaves differently in these two modes, which has same timings?

Thanks,
PG