For the DDR_CK trace, there are two input cell for two x8 memories.
If one x16 memory is used, is only the cell on row of "Byte 0" used?
Is the cell on row of "Byte 1" a blank?
The trace length is set in inches.
Can the decimal point be used?
Best regards,
Daisuke