Dear All,
We are working on TI8148 Processor which has Arm-Cortex A8 and C674x DSP Core.
We are communicating between ARM and DSP via RINGIO's created from syslink.
Whenever there is a data communication between Two RingIo's (Rx and Tx) simultaneously, we are observing the following problems:
- Kworker is consuming lot of CPU load(20-30%)
- Our application also consuming similar amount of CPU load(20-30%)
So, can you please help us in debugging this issue. Is it a problem with the syslink module?
Please find the different modules and its version, that I am using:
bios - 6.33.02.31
biospsp - 3.10.5.0
xdais - 7.21.0.2
XDCtools - 3.23.01.43
syslink - 2.21.01.05
Best Regards,
Shankaralingam. Ga