I can successfully compile and run the "client" example for my EVM6678 board. I am able to access the board from my PC connected on the same network.
My question is what are the commands I need to add to the "client" example to send / receive data packets through the ethernet port from the EVM6678 board. I am trying to exchange data between the PC and the EVM6678.
Is another example perhaps more suited?