Hi guys,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi guys,
Hi.
1) I did the same question on pandaboard Google group and i solved the problem. Here is the link : https://groups.google.com/forum/#!topic/pandaboard/QZ3eLi67jaU.
2)if i got what you mean, you don't have any linux host to flash the SD card , do you? if so install linux on a VM in a Windows or MacOS pc. Did you buy Chipsee LCD touchscreen for your pandaboard?
Hi Giorgio,
Thanks for the answer.
And yes I buy one for my Pandaboard. Sincerely I refuse install VM on my MAC, time ago I have many troubles with Virtualbox and finally I need to reinstall the entire OSX. In MAC I can flash an image via dd command, I usually do that for Pandas and Beagle boards, but I need an prebuild image, in the case of Chipset companion disk the image need to be composed running an script that is possible only in a Linux box.
Cheers.
You are right, Hector.....Virtual box, in my MAC, gave my a lot of pain too. Finally i installed VMWARE. It works like a charm. it could be extreme but (for my robotics project) i did also a dual boot on my macbook with ubuntu 12.04 without problems. however it's hard to find some "Cheepse prebuild" around the web.
Try...maybe you're lucky.
Bye!