This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Add video capture function in DM8168 issue

WinCE BSP version :BSP_WINCE_ARM_A8_02_30_00 

wince hdvpss M3 firmware version : 01000126

Linux BSP Version :ti-ezsdk_dm816x-evm_5_05_02_00,linux-2.6.37-psp04.04.00.01

Linux hdvpss M3 firmware version:01000137

i want to port linux capt module to wince7 , now ,code porting is finished , but blocking in init capt module, after some debug , i found the wince M3 firmware is not match with capt module from linux , as you know , linux capt module is based on 01000137 M3 firmware , but wince side is 01000126 . so , in my opinion , there should be some mismatch in parameters transfer ,such as Vps_CaptCreateParams, Vps_VipPortConfig,Vps_VipConfig in share mem offset .

so , i think if anyone can give me the linux hdvpss code based on M3 firmware 01000126 is the best way for porting .

if not , maybe i must rebuild hdvpss for wince , then  i can define the share mem address ,and get ti816x_hdvpss.xem3.map