Hi,
I'm using SYS/BIOS on AM335x EVM and want to use ROV for debug purpose.
When I launched ROV in CCSv5.3 , I saw the same error reported in http://e2e.ti.com/support/arm/sitara_arm/f/791/p/189950/681695.aspx#681695
The error said that something path might be wrong, but please note I have confirmed I could use ROV with the same RTSC-ed packages/package path on C674x target board. Also, I tried to
- relaunch target configuration
- reboot CCS
to see if the problem was disappeared or not, but the it is still there.
So now, question - is ROV supported for AM335x device on CCSv5.3?
I'm asking this because there is not valid answer in http://e2e.ti.com/support/arm/sitara_arm/f/791/p/189950/681695.aspx#681695
about ROV usability.
Lastly, my environment looks like below:
- CCSv5.3
- SYS/BIOS 6.34.4.22 (installed to default path, i.e., C:\ti)
- XDCTool 3.24.5.48 (installed to default path, i.e., C:\ti)
- RTSC parameters
- Target : ti.target.arm.elf.A8Fnv
- Platform: ti.platforms.evmAM3359
- Build-profile: release
Kawada