HI, This is regarding the chip finalizing for our new project. The below is a partially requirement, Should Run Linux(Cent) OS on the chip. Should support X11 protocol for Display data communication. The price should be within $25-45. Should support already running application on intel 64bit processor at client location to our newly finalizing chip. Others are lot of IO’s and Sensors controllers. I needed a perfect chip which has all above features and complete support from your end like libraries, starter kit, etc.
Can any one tell me a 64/32bit procesors.
Regards Sridharan J