I am new to CCS and Configuration Tool. I use CCS5, Configuration Tool v 5.00 and EZDSP5502.
In all the documents I have read it is written that after the setup with configuration tool, .cmd and .cdb files must have been generated. I have not seen a button or a shortcut on the configuration tool window. After building the project, these files didn't show up either. Except the following error I have not seen any errors:
..../tconf: batch mode specified but no script file was supplied.
Then comes some usage tips and
gmake: *** [<task>cfg.cmd] Error 1
gmake: Target 'all' not remade because of errors.
**** Build Finished ****
When the project is run in debug mode, you can see that build is not actually finished, but there are some problems. <task>.out cannot be opened. I guess I have a problem with configuration tool or experiencing some compatibility problems.