Hi,
we are using two types of custom build hardware, which are using the C6414 or C6415 DSPs. The problem is that the profile clock doesn't work with one of these boards. I'm getting different behaviour for different Emulators or CCS Versions:
- CCS V3.3, SD XDS510 USB:
"Error enabling a profile counter: Profiling not supported with existing configuration. Check that Advanced Event Triggering components are enabled." - CCS V5.4, SD XDS510 USB:
Profile Clock menu is not available (greyed out) - CCS V5.4, SD XDS560v2 LC:
"Error enabling a profile counter"
The strange thing is that the profile clock works without any problems, if I follow these steps:
- Restart CCS V3.3 or CCS V5 Debug Session
- Connect first to the hardware which normally works without a problem
- Disconnect again
- Connect to the hardware which normally causes problems
- Enable Profile Clock
If I first connect to the hardware which is causing the problems instead, the other hardware will also not work until CCS or the Debug session is restarted. Something seems to be different when CCS establishes the first connection to the DSP.
Any ideas?
Thanks,
Ralf