Other Parts Discussed in Thread: AM3358, TMDXEVM3358
Hi.
I'm using the AM3358 sample board, please tell me the setting of XLDRNOR.nb0 of Windows Embedded Compact 7.
1. If I build an environment of "\ BOOTLOADER \ XLDR \ NOR" folder of AM35x BSP, XLDRNOR.nb0 that can be NOR boot or be generated.
2. Writing to address 0x08000000 the XLDRNOR.nb0 I was produced in 1., Does it do NOR boot.
3. I believe GP Image Header that's not required for the XLDRNOR.nb0. Is it correct.
4. Is there any settings that are different from the NAND boot in GP Image Header other than.
Terry Yam