i made a custom board,it chip is AM3894,the DDR2 work on 400MHz,
when capture video with the resolution 640*480,it works very well。
when i change the resolution more than 800*600,there is nothing display on monitor, but if i stop the video input source,the monitor display the a frame of video。
is the problems caused by low bandwidth of DDR2。
please give some suggestions about the problem。