Hello,
We are designing a HD capture solution on DM8168, DVR RDK 4.0.
Our HD capture sources have different interlaced mode such as 1080I and 720P, so we connect capture link to a select link to choose different dei links. However, it seems that select link drops some frames if the input sources are 1080I and 720P. How can I avoid this problem? Thank you very much.
As below statistics, capture FPS are 60 and 59, but Recv. FPS of DEI0 and DEI1 (which is behind select link) are 36 and 45. Without select link, the Recv. FPS is normal.
[m3vpss ] CH | Fields Fields Fields FPS FPS FPS Width Height Fields Count (Desc Error Y/C)
[m3vpss ] ------------------------------------------------------------------------------------------------------------
[m3vpss ] 000 | 18132 18132 0 60 60 0 1280 / 1280 720 / 720 7217 0 0/0 (0/0)
[m3vpss ] 200 | 17875 8943 8932 59 29 29 1920 / 1920 277 / 576 4052 11 0/0 (0/0)
[m3vpss ] *** [DEI0 ] DEI Statistics ***
[m3vpss ]
[m3vpss ] Elasped Time : 300 secs
[m3vpss ] Total Fields Processed : 10834
[m3vpss ] Total Fields FPS : 123 FPS
[m3vpss ]
[m3vpss ]
[m3vpss ] CH | In Recv In Reject In Process Out[0] Out[1] Out[2] Out[3] Out[4] Skip Out[0] Skip Out[1] Skip Out[2] Skip Out[3] Skip Out[4] User Out[0] User Out[1] User Out[2] User Out[3] Use
[m3vpss ] Num | FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS Skip FPS Skip FPS Skip FPS Skip FPS Sk
[m3vpss ] --------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 36 0 36 18 0 0 0 0 0 36 0 0 0 18 0 0 0 8
[m3vpss ]
[m3vpss ]
[m3vpss ] *** [DEI1 ] DEI Statistics ***
[m3vpss ]
[m3vpss ] Elasped Time : 300 secs
[m3vpss ] Total Fields Processed : 10168
[m3vpss ] Total Fields FPS : 49 FPS
[m3vpss ]
[m3vpss ]
[m3vpss ] CH | In Recv In Reject In Process Out[0] Out[1] Out[2] Out[3] Out[4] Skip Out[0] Skip Out[1] Skip Out[2] Skip Out[3] Skip Out[4] User Out[0] User Out[1] User Out[2] User Out[3] Use
[m3vpss ] Num | FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS FPS Skip FPS Skip FPS Skip FPS Skip FPS Sk
[m3vpss ] --------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------
[m3vpss ] 0 | 45 11 33 16 0 0 0 0 0 33 0 0 0 16 0 0 0 4
+--------------+
| |
| |
| Capture |
| |
| |
+--------------+
+
|
| 2ch HD
|
V
+--------------------------+
| |
| Select |
| |
+----+-----------+-------+
| |
0| |1
| |
v v
+---------+ +-----------+
| | | |
|DEI | | DEI |
|Bypass | |Enabled |
+--------+ +------------+
+ +
| |
v v
+-----------------+
| |
| nsf |
| |
+-----------------+