This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCSDK 2.01.02.06 IBL build errors

I originally posted this in the Keystone forum, but this may be the more appropriate place.

http://e2e.ti.com/support/dsp/c6000_multi-core_dsps/f/639/t/269182.aspx

 

When trying to build the evm_c6657_spi target in the IBL directory of the MCSDK 2.01.02.06 , I get the below error. It seems like this build target has not been tested. Is this target supported?

/opt/ti/mcsdk_2_01_02_06/tools/boot_loader/ibl/src/make# make evm_c6657_spi
rm -f ../util/symExtract/symExtract_unix
cat ibl_c665x/ibl_objs_template.inc | sed -e s/ENDIAN_TAG/le/g > ibl_c665x/ibl_objs.tmp
cl6x -ppo -DIBL_CFG_I2C_MAP_TABLE_DATA_BUS_ADDR=0x51 -DEXCLUDE_I2C -DENDIAN_TAG=le ibl_c665x/ibl_objs.tmp
cp -f ibl_c665x/ibl_objs.pp ibl_c665x/ibl_objs.inc
cl6x -z -o ibl_c665x/ibl_c665x.out -m ibl_c665x/ibl_c665x.le.map  ibl_c665x/ibl.cmd /opt/ti/ccsv5/tools/compiler/c6000_7.4.2/lib/rts64plus.lib
<Linking>
error: symbol "_hwDevInfo" redefined: first defined in
   "../hw/c64x/make/nandemif25.le.oc"; redefined in
   "../hw/c64x/make/nandgpio.le.oc"
error: errors encountered during linking; "ibl_c665x/ibl_c665x.out" not built


>> Compilation failure
make[2]: *** [iblMain] Error 1
make[2]: Leaving directory `/opt/ti/mcsdk_2_01_02_06/tools/boot_loader/ibl/src/make'
make[1]: *** [le_target] Error 2
make[1]: Leaving directory `/opt/ti/mcsdk_2_01_02_06/tools/boot_loader/ibl/src/make'
make: *** [evm_c6657_spi] Error 2

  • David,

    Someone from the MCSDK apps team has been assigned to look at this and get back to you…

    Scott

  • Scott, thanks for the follow up. I look forward to receiving an answer.

     

  • Hello, issue you reported has been reproduced. we will provide an update to you soon.

    regards,

    David

  • To fix this issue, please make the following two changes in the build file:

    1) <IBL_INSTALL_DIR>/src/hw/c64x/make/makefile

          Change line #71 from "CSRC+= nandemif25.c nandgpio.c spi.c nandspi.c noremif25.c norspi.c emif25.c spiutil.c c66x_uart.c" to "CSRC+= nandemif25.c spi.c nandspi.c noremif25.c norspi.c emif25.c spiutil.c c66x_uart.c"

    2) <IBL_INSTALL_DIR>/src/make/Makefile

        Change line #345 from "make -f makestg1 ARCH=c64x TARGET=c665x I2C=no I2C_BUS_ADDR=0x51 I2C_MAP_ADDR=0x500 ENDIAN_MODE=little CEXCLUDES=I2C SPI_DEFS='$(EVM_667x_SPI_DEFS)' c66x" to "make -f makestg1 ARCH=c64x TARGET=c665x I2C=no I2C_BUS_ADDR=0x51 I2C_MAP_ADDR=0x500 ENDIAN_MODE=little CEXCLUDES='I2C NAND_GPIO' SPI_DEFS='$(EVM_667x_SPI_DEFS)' c665x"

     

    regards,

    David