1) is the hardware really pin for pin compatible as advertised?
2) is the core software compatible as advertised?
3) what kind of speed increases can we expect in encoding and gpu performance?
Regards,
-Jaden
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1) is the hardware really pin for pin compatible as advertised?
2) is the core software compatible as advertised?
3) what kind of speed increases can we expect in encoding and gpu performance?
Regards,
-Jaden
Jaden,
1) Yes. You can even drop-replace DM369 on a DM368 PCB for you to test
2) Yes. The difference is that DM369 is capable of running TI's 3rd generation noise filtering for low-light
3) The main performance difference is the capability of running the advanced low-light noise filter via hardware acceleration. Other DM368 components will still run at the same good quality on the DM369 silicon
Jaden,
DM368 and DM369 run on same clock frequencies and are pin-to-pin compatible
Arm is at 432Mhz and DDR at 340Mhz
Regards,
Raghu
Hello,
DM369 is targeted for new third generation improved noise filter along with DM368 functionality.
DM369 runs on same clock freq as that DM368 and is pin-to-pin compatible.
So DVSDK should run on DM369 too as DVSDK does not have Noise FIlter in it
What that the query you were looking for?
Regarding DVSDK releases, please check with local sales to get all the details
Regards,
Raghu
Hello Bob,
DM369 is designed to add third generation noise filter functionality on top of DM368.
If you are not using Noise Filter, then DM368 and DM369 is same
Regards,
Raghu
Although the TI website points to DVSDK 4.03.00.06 as the latest release for the DM368, there is no DM368 download available on that page. PSP 3.21.00.04 supports the DM368 and has the 2.6.37 Linux kernel that is apparently in the DVSDK 4.03 but lacks the supporting components the are part of the DVSDK. There are features in Linux 2.6.37 and later that would be very beneficial to my application. I hoped that announcement of the DM369 would mean updates to the DVSDK were in the works. At a minimum, I'd like a way to get a complete DVSDK 4.03 package for the DM368.
Thanks,
-Carl