This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with Fastboot on am335xevm_sk running JellyBean

Hi,

I'm trying to boot an image using fastboot but it's stalling without any error.

From the device I can start fastboot correctly: 

U-Boot# fastboot
INFO: [do_fastboot]: fastboot initialized
INFO: [fbt_init_endpoints]: setting up HS USB device ep1
INFO: [fbt_init_endpoints]: setting up HS USB device ep82
Invalid string index 238

And on the host I can query the device correctly:

$ fastboot devices
???????????? fastboot

But I can't do anything else. Every other commands get stuck like the following:

$ fastboot boot boot.img
downloading 'boot.img'...

It's staying like this forever until I reboot the target.

Any idea?