Other Parts Discussed in Thread: TPS65217, ISO1050
I have a Bone and evm SK I followed this here http://processors.wiki.ti.com/index.php/AMSDK_Linux_User%27s_Guide
I dont see all the def_configs listed in this doc? did I grab the wrong SDK?
in my tree I downloaded the Bone SDK all I saw was the tisdk_am335x-evm_defconfig
I did a make linux
Do I need to set any jumpers and which board should I try this image on the Bone or EVM ? I looked at Bone quick start and it apppears it boots over ethernet do I need a cross over cable or a switch. It seems like since I am newbie I probally should use prebuilt Bone images to get started
Please give me a push start for Bone I would eventually like the kernel that support the CAN capes I have a white Bone
Thanks