Other Parts Discussed in Thread: AM1808
Hello,
I'm using Linux 03.20.00.14 on SBC8018 development board (AM1808) and I need to enable one GPIO (44th) pin.I would like to use "uP_SPI1_ENAN" pin (11th pin on J42 expasion board) as GPIO. I added this code for multiplexing, and I hope that this is OK:
MUX_CFG(DA850, GPIO2_12, 5, 12, 15, 8, false); // This is 44th pin when I use it from userspace?
Also, I selected in menuconfig:
Device drivers --->
-*- GPIO support --->
[*] /sys/class/gpio/... (sysfs interface)
Is this enough?
I would like to read that GPIO pin from my application. How to do it?
Best regards,
Vladimir