Other Parts Discussed in Thread: AM3359
We are designing a board with AM3359 (ZCZ) and DDR3 (one chip), and facing some difficulties in component selection.
What we want to know is the possibles combinations of the 2 chips.
1 - Reading the DS (table 3.6) it seems tha the only mode to support DDR3 is OPP100 at 400 MHz. Is it correct? If not what is correct?
2 - Reading further (table 3.7) it seems that OPP100 is only supported for Sitaras of 300 and 600 MHz grades. Is it correct? If not what is correct?
3 - What procedure to follow to adapt the DR3 to the Sitara in terms of speed including the multipliers and dividers of the formula bellow:
DDR_CLK frequency = (DDRPLL input clock frequency x mulitplier)/((pre-divider+1)*post-divider)
Suppose we are trying to use the fastest combination possible of the two chips.
Thank you!
Luis