This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dvtb capture issue

I am trying to use dvtb to capture and encode using imgenc1. 

I am using dm6467T EVM with:

dvsdk_3_10_00_19

cs2dm6467_1_00_00_10

codec_engine_2_25_05_16

framework_components_2_25_02_06

Below is the output of executing the dvtb script.  Any ideas as to why /dev/video0 cannot be initialized? It seems that the standard parameter for the vpfe is incorrect no matter what I pick.  I've tried 0 through 3 based on the DVTB User's guide, but they all result in the same error.   For sanity's sake, I am able to run the encodedecode demo which I believe uses /dev/video0 as the capture device.

./dvtb-r -s dvtb_script.sh
@0,560,636us: [+6 T:0x4001f390] CE - Engine_init> CE debugging on (CE_DEBUG=1; allowed CE_DEBUG leve)

# codec engine
 
#setp engine name encodedecode
 

# codec
 
setp imgenc1 codec jpegenc
 PASS: setp


# image encoder parameters
 
setp imgenc1 maxHeight 576
 PASS: setp

setp imgenc1 maxWidth 720
 PASS: setp

setp imgenc1 maxScans 0
 PASS: setp

setp imgenc1 dataEndianness 1
 PASS: setp

settvp7002 1-005d: Invalid id...
p imgenc1 forceChromaFormat 2
 PASS: setp

setp imgenc1 numAU 0
 PASS: setp

setp imgenc1 inputChromaFormat 4
 PASS: setp

setp imgenc1 inputHeight 480
 PASS: setp

setp imgenc1 inputWidth 720
 PASS: setp

setp imgenc1 captureWidth 720
 PASS: setp

setp imgenc1 generateHeader 0
 PASS: setp

setp imgenc1 qValue 73
 PASS: setp


# vpfe parameters
 
setp vpfe device /dev/video0
 PASS: setp

setp vpfe standard 1
 PASS: setp

setp vpfe format 1
 PASS: setp

setp vpfe input 0
 PASS: setp

setp vpfe width 720
 PASS: setp

setp vpfe height 480
 PASS: setp


func imgenc1 -t test.jpg
 [DVTB-LOG]: linux/dvtbFuncDispatcher.c: Starting Thread for command <imgenc1>
[DVTB-LOG]: ../core/linux/dvtbUtils.c: Image [capture]+[encode] usecase started
[DVTB-ERROR]: VIDIOC_S_STD failed for <1> format for </dev/video0>
Error :: Invalid argument
[DVTB-ERROR]: linux/dvtbImgCapture1.c: Unable to initialize VPFE device </dev/video0>
[DVTB-LOG]: ../core/linux/dvtbImgCapture1Core.c: Total # of Slices Encoded = 0
[DVTB-LOG]: ../core/linux/dvtbImgCapture1Core.c: Image Encoder <jpegenc> closed
[DVTB-LOG]: ../core/linux/dvtbImgCapture1Core.c: Engine <encodedecode> closed
[DVTB-LOG]: ../core/linux/dvtbUtils.c: Image [Capture]+[Encode] usecase completed with errors.
PNDG: func