This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSI suppot in DM8148

I have a customer asking the following question. 

In the DM8148 evm schematic has the CSI interface on page 25; but those pins are RSV6 - RSV14 in the data sheet. My question is, does the DM8148 support CSI interface?

  • Hi Hector,

    The data sheet is correct for the DM devices.

    Currently CSI2 is not supported in software so references to CSI2 have been removed from the data sheet. CSI2 is supported in hardware.

    The schematics are more generic than the data sheet.

    See also the below thread:

    http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/716/t/254368.aspx

    BR

    Pavel