Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ROV Unknown error on startup

Other Parts Discussed in Thread: SYSBIOS, AM3359

I updated a CCS5.3 installation to CCS5.4 on a Pentium 4 XP machine.

My application loads and runs fine.  When I break, and bring up ROV, it displays "Unknown error".

How can I find out what is wrong so I can fix it? 

I did find an older post regarding a C6000 with a similar symptom, but I have the Window->Preferences RTSC configured as shown there.

I also have a new Windows 7 CCS5.4 install, same target code and configuration, in which ROV works.

The platform is AM3359 (BeagleBone), Compiler 5.05, SYSBIOS 6_35_01_29, xdctools_3_25_00_48.  Debugging via the built in XDS100v2.

Gerry Belanger

  • Hi Gerry Belanger,

    Maybe it's a memory problem?  How much RAM do you have on your WinXP machine?

    When you see the problem, can you see how much heap is being used by Code Composer?  You can see the heap status by setting Window -> Preferences -> General -> Show heap status:

    Steve

  • Steve,

    The PC has 2.5GB of memory. 

    Heap shows 65M of 116M when the  ROV window opens and shows the error.

    Before I upgraded to CCS 5.4 and XDC 3.25, ROV worked on this machine.

    Gerry Belanger

  • Steve,

    I just noticed a discrepancy in versions.  In the Help->About Code Composer Studio-> Installation Details, the XDC version is 3.25.0.48, as expected.

    But if I look at Help->About Code Composer Studio-> RTSC, it shows 3.24.7.73, the version I used with CCS 5.3.

    So it looks like something did not get updated during the upgrade.

    Any ideas as to how to correct this?

    GerryB

  • Steve,

    This issue is now moot.  I tried removing the old XDC tools, but that caused build problems.  So I bit the bullet, so to speak.

    I totally uninstalled CCS and the TI drivers, then re-installed CCS 5.4 from the offline installer.  After applying the available updates, I was able to build my target, download it and pull up ROV.

    I wouldn't call it an elegant solution, but it worked.

    Gerry Belanger

  • Ok, glad you resolved the issue but not so glad that you had to reinstall CCS to get there.

    My next suggestion would have been to try changing your settings to different versions of XDCtools, trying ROV with each one.  Maybe if it happens again you could try that.

    Steve