Hello:
I inherited a seemingly new AM335x Evaluation Module for an ex-employee. I have been tasked to get a Windows CE7 image to load on it, I have spent several hours going through the documented steps to get an image to boot from both SD and the Uart. but so far nothing seems to be working for me.
In fact I can't seem to get past the 'C' output.
So I found the Linux SD card that came with the unit. I was hoping that this would boot to the Linux desktop, but it does not. after several 'C's I do get loader output and I can get into a menu. But when I just let the device try to boot the image I get a error message indicating that the image is not formatted correctly.
I also noticed that on my Win7 desktop I can not read the Linux boot SD is that normal?
any suggestions would be appreciated.
Mark