Other Parts Discussed in Thread: SYSBIOS, TMS320F28062
Hi,
I am actually evaluating possibility to use sysbios (6.35.1.29) on a TMS320f28062 (clk=90MHz) to drive a power supply. In my basic program, I use
- One low priority task toggling one output,
- One clock (swi) posting a semaphore to access an high priority task. This second task toggles a second ouput.
If I choose Tick period & Clock period between 100us and 1ms, it seems that the OS begin to have some difficulties to follow. I can see that because my low priority task is almost never called and my high priority task shows a non-periodic access (meaning that Tick period is lower than semaphore treatment latency). - Checked via oscillo connected to outputs -
My target is to periodically call functions that would launch actions like ADC conversion and result treatment with an approximate period of 100us. This with other tasks that must have a maximum latency below 5ms. Can I do that with SYSbios? (I hope yes!).
Many thanks for your feedback.