This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unable to communicate between OMAP 3530 and C6678

Other Parts Discussed in Thread: MIDAS, OMAP3530, ADS7846, TVP5146M2

Hi
I am woriking on midas v4.0 to run the demo by integrating omap and C6678 using sdcard image. For C6678 I am using mcsdk_2_01_02_05 and prebuit images given at https://gforge.ti.com/gf/project/med_ultrasound/frs/?action=FrsReleaseBrowse&frs_package_id=267. Neither I am unable to communicate between OMAP and C6678, C6678 and my Windows PC. I am using D-Link 5 port gigabit Network switch. The following is being displayed in the console.
[C66xx_0] HEAPID = 3
[C66xx_0] IPADRESS is = 192.168.3.202
[C66xx_0] Mid End process started
[C66xx_0] MidEnd_gatherTask started
[C66xx_0] Successfully created BPU instance
[C66xx_0] Successfully created DPU instance

Thanks

  • Hi Akkala

    Could you please provide the complete log from the time the OMAP3530 boots, as well as the Code Composer Studio console log for the 6678 side?

  • Hi uday

    the console of Code Composer Studio was showing only

    [C66xx_0] HEAPID = 3
    [C66xx_0] IPADRESS is = 192.168.3.202
    [C66xx_0] Mid End process started
    [C66xx_0] MidEnd_gatherTask started
    [C66xx_0] Successfully created BPU instance
    [C66xx_0] Successfully created DPU instance 

    the console of OMAP3530 was displaying 

    I was able to see the image from SD card onto external display but the image was not clear and no communication is being established between OMAP3530 and C6678.

    Thanks 

  • Akkala,

    The reason you see the processed image on the screen despite there being a failed communication between 6678 and OMAP3530, is that the demo runs in OMAP-only mode when it can't find the 6678. The OMAP-only mode means that all algorithms run on the OMAP3530's C64x+ DSP. 

    To further debug the reason for 6678 and OMAP3530 not communicating, could you please provide the complete log on the OMAP3530, right from the time the OMAP boots with x-loader, etc?

    Also if you could do a 'printenv' when you get the uboot prompt, that would help us see the boot parameters.

  • Hi Uday,

    The below is the complete log of OMAP3530

    Texas Instruments X-Loader 1.46 (Jan 12 2011 - 23:48:51)                    
    Starting X-loader on MMC                                                    
    Reading boot sector                                                         
                                           
    212880 Bytes Read from MMC             
    Starting OS Bootloader from MMC...     
    Starting OS Bootloader...              
                                           
                                           
    U-Boot 2009.11 (Jan 12 2011 - 23:49:00)

    OMAP3430/3530-GP ES3.1, CPU-OPP2 L3-165MHz
    OMAP3 EVM board + LPDDR/NAND                                                   
    I2C:   ready                                                                   
    DRAM:  128 MB                                                                  
    NAND:  256 MiB                                                                 
    In:    serial                                                                  
    Out:   serial                                                                  
    Err:   serial                                                                  
    Read back SMSC id 0x92200000                                                   
    Die ID #519600040000000004036abb0300a008                                       
    Net:   smc911x-0                                                               
    Hit any key to stop autoboot:  8
    OMAP3_EVM # setenv bootargs console=ttys0,115200n8 rw mem=99M@0x80000000 mpurate=720 mem=100M@0x89300000 omap_vout.vidl_static_vrfb_alloc=y omapfb.vram=0:3 omapfb.mode=dvi:1280x720@60 root=/dev/mmcblk0p2 f
    OMAP3_EVM # setenv bootcmd 'mmc init [dev/ttyUSB0];fatload mmc 0 0x82000000 uImage;bootm 0x82000000'

    After printenv

    bootdelay=10
    baudrate=115200
    bootfile=uImage
    loadaddr=0x82000000
    usbtty=cdc_acm
    console=ttyS2,115200n8
    mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
    nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2
    loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
    bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
    loaduimage=fatload mmc 0 ${loadaddr} uImage
    mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
    nandboot=echo Booting from nand ...; run nandargs; onenand read ${loadaddr} 280000 400000; bootm ${loadaddr}
    dieid#=519600040000000004036abb0300a008
    ethact=smc911x-0
    stdin=serial
    stdout=serial
    stderr=serial
    bootargs=console=ttys0,115200n8 rw mem=99M@0x80000000 mpurate=720 mem=100M@0x89300000 omap_vout.vidl_static_vrfb_alloc=y omapfb.vram=0:3 omapfb.mode=dvi:1280x720@60 root=/dev/mmcblk0p2 rootfstype=ext3 roof
    bootcmd=mmc init [dev/ttyUSB0];fatload mmc 0 0x82000000 uImage;bootm 0x82000000

    OMAP3_EVM #boot

    Then i got the following on the console

    Environment size: 1010/131068 bytes
    OMAP3_EVM # boot
    mmc0 is available
    reading uImage

    2400552 bytes read
    ## Booting kernel from Legacy Image at 82000000 ...
       Image Name:   Linux-2.6.32
       Image Type:   ARM Linux Kernel Image (uncompressed)
       Data Size:    2400488 Bytes =  2.3 MB
       Load Address: 80008000
       Entry Point:  80008000
       Verifying Checksum ... OK
       Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux........................................................................................................................................................ done, booting the kernel.

    Then the image is being displayed on the screen but no communication has been established with C6678.

    Thanks

  • Hi

    can anyone help me out of this issue i have been waiting for answer from many days but there has been no reply.

    thanks

    vivek akkala

  • Hi Vivek

    From the log you provided in your previous post, it looks like there are some arguments missing in the bootargs. When you did a printenv, it does not show the following two arguments highlighted in yellow below:

    bootargs console=ttyS0,115200n8 rw mem=99M@0x80000000 mpurate=720 mem=100M@0x89300000 omap_vout.vid1_static_vrfb_alloc=y omapfb.vram=0:3M omapfb.mode=dvi:1280x720@60 root=/dev/mmcblk0p2 rootfstype=ext3 rootwait ip=off

    Could you please correct the bootargs as above and try again? 

    If the problem is not solved with the above, please go to your NFS directory to the path etc/init.d/rcS and comment out the line that calls 'ultrasound -qws.' Then boot the board. Once it reaches the linux command prompt, try to 'ping' the IP address of the 6678, and let us know if the ping works or not.

    Also please provide the complete log. Right from the beginning to the end, including bootargs, the kernel decompressing, the ultrasound demo being launched, everything. 

    Thanks.

  • Hi uday 

    Thanks for responding. I am having the same problem after including rootwait ip=off in bootargs

    The complete log is as below

    Texas Instruments X-Loader 1.46 (Jan 12 2011 - 23:48:51)
    Starting X-loader on MMC
    Reading boot sector

    212880 Bytes Read from MMC
    Starting OS Bootloader from MMC...
    Starting OS Bootloader...


    U-Boot 2009.11 (Jan 12 2011 - 23:49:00)

    OMAP3430/3530-GP ES3.1, CPU-OPP2 L3-165MHz
    OMAP3 EVM board + LPDDR/NAND
    I2C: ready
    DRAM: 128 MB
    NAND: 256 MiB
    *** Warning - bad CRC or NAND, using default environment

    In: serial
    Out: serial
    Err: serial
    Read back SMSC id 0x92200000
    Die ID #519600040000000004036abb0300a008
    Net: smc911x-0
    Hit any key to stop autoboot: 0
    OMAP3_EVM # print
    bootcmd=if mmc init; then if run loadbootscript; then run bootscript; else if run loaduimage; then run mmcboot; else run nandboot; fi; fi; else run nandboot; fi
    bootdelay=10
    baudrate=115200
    bootfile=uImage
    loadaddr=0x82000000
    usbtty=cdc_acm
    console=ttyS2,115200n8
    mmcargs=setenv bootargs console=${console} root=/dev/mmcblk0p2 rw rootfstype=ext3 rootwait
    nandargs=setenv bootargs console=${console} root=/dev/mtdblock4 rw rootfstype=jffs2
    loadbootscript=fatload mmc 0 ${loadaddr} boot.scr
    bootscript=echo Running bootscript from mmc ...; source ${loadaddr}
    loaduimage=fatload mmc 0 ${loadaddr} uImage
    mmcboot=echo Booting from mmc ...; run mmcargs; bootm ${loadaddr}
    nandboot=echo Booting from nand ...; run nandargs; onenand read ${loadaddr} 280000 400000; bootm ${loadaddr}
    stdin=serial
    stdout=serial
    stderr=serial
    dieid#=519600040000000004036abb0300a008
    ethact=smc911x-0

    Environment size: 874/131068 bytes
    OMAP3_EVM # setenv bootargs console=ttyS0,115200n8 rw mem=99M@0x80000000 mpurate=720 mem=100@0x89300000 omap_vout.vid1_static_vrfb_alloc=y omapfb.vram=0:3M omapfb.mode=dvi:1280x720@60 root=/dev/mmcblk0p2 rootfstype=ext3 rootwait ip=off
    OMAP3_EVM # setenv bootcmd 'mmc init;fatload mmc 0 0x82000000 uImage;bootm 0x82000000'
    OMAP3_EVM # boot

    mmc1 is available
    reading uImage

    2400552 bytes read
    ## Booting kernel from Legacy Image at 82000000 ...
    Image Name: Linux-2.6.32
    Image Type: ARM Linux Kernel Image (uncompressed)
    Data Size: 2400488 Bytes = 2.3 MB
    Load Address: 80008000
    Entry Point: 80008000
    Verifying Checksum ... OK
    Loading Kernel Image ... OK
    OK

    Starting kernel ...

    Uncompressing Linux.....................................................................................................................................................

    Linux version 2.6.32 (uday@LTA0132923-LINUX) (gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203) ) #1 Thu Jan 27 17:01:09 CST 2011
    CPU: ARMv7 Processor [411fc083] revision 3 (ARMv7), cr=10c53c7f
    CPU: VIPT nonaliasing data cache, VIPT nonaliasing instruction cache
    Machine: OMAP3 EVM
    Memory policy: ECC disabled, Data cache writeback
    OMAP3430/3530 ES3.1 (l2cache iva sgx neon isp )
    SRAM: Mapped pa 0x40200000 to va 0xfe400000 size: 0x100000
    Reserving 4194304 bytes SDRAM for VRAM
    Built 1 zonelists in Zone order, mobility grouping on. Total pages: 25146
    Kernel command line: console=ttyS0,115200n8 rw mem=99M@0x80000000 mpurate=720 mem=100@0x89300000 omap_vout.vid1_static_vrfb_alloc=y omapfb.vram=0:3M omapfb.mode=dvi:12f
    PID hash table entries: 512 (order: -1, 2048 bytes)
    Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
    Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
    Memory: 99MB = 99MB total
    Memory: 91348KB available (4192K code, 372K data, 172K init, 0K highmem)
    Hierarchical RCU implementation.
    NR_IRQS:402
    Clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
    Reprogramming SDRC clock to 332000000 Hz
    GPMC revision 5.0
    IRQ: Found an INTC at 0xfa200000 (revision 4.0) with 96 interrupts
    Total of 96 interrupts on 1 active controller
    OMAP GPIO hardware version 2.5
    OMAP clockevent source: GPTIMER1 at 32768 Hz
    Console: colour dummy device 80x30
    Calibrating delay loop... 597.64 BogoMIPS (lpj=2334720)
    Mount-cache hash table entries: 512
    CPU: Testing write buffer coherency: ok
    regulator: core version 0.5
    NET: Registered protocol family 16
    This silicon doesn't support 720MHz
    Target VDD1 OPP = 5, VDD2 OPP = 3
    omap3evmdc: Driver registration complete
    OMAP DMA hardware revision 4.0
    bio: create slab <bio-0> at 0
    SCSI subsystem initialized
    usbcore: registered new interface driver usbfs
    usbcore: registered new interface driver hub
    usbcore: registered new device driver usb
    i2c_omap i2c_omap.1: bus 1 rev3.12 at 2600 kHz
    twl4030: PIH (irq 7) chaining IRQs 368..375
    twl4030: power (irq 373) chaining IRQs 376..383
    twl4030: gpio (irq 368) chaining IRQs 384..401
    regulator: VMMC1: 1850 <--> 3150 mV normal standby
    regulator: VDAC: 1800 mV normal standby
    regulator: VAUX2_4030: 2800 mV normal standby
    regulator: VPLL2: 1800 mV normal standby
    regulator: VSIM: 1800 <--> 3000 mV normal standby
    i2c_omap i2c_omap.2: bus 2 rev3.12 at 400 kHz
    i2c_omap i2c_omap.3: bus 3 rev3.12 at 400 kHz
    Switching to clocksource 32k_counter
    musb_hdrc: version 6.0, musb-dma, otg (peripheral+host), debug=0
    musb_hdrc: USB OTG mode controller at fa0ab000 using DMA, IRQ 92
    NET: Registered protocol family 2
    IP route cache hash table entries: 1024 (order: 0, 4096 bytes)
    TCP established hash table entries: 4096 (order: 3, 32768 bytes)
    TCP bind hash table entries: 4096 (order: 2, 16384 bytes)
    TCP: Hash tables configured (established 4096 bind 4096)
    TCP reno registered
    UDP hash table entries: 256 (order: 0, 4096 bytes)
    UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
    NET: Registered protocol family 1
    RPC: Registered udp transport module.
    RPC: Registered tcp transport module.
    RPC: Registered tcp NFSv4.1 backchannel transport module.
    omap-iommu omap-iommu.0: isp registered
    OMAP35x Linux PSP version 03.00.01.06 (OMAP3EVM)
    NetWinder Floating Point Emulator V0.97 (double precision)
    VFS: Disk quotas dquot_6.5.2
    Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
    JFFS2 version 2.2. (NAND) �© 2001-2006 Red Hat, Inc.
    msgmni has been set to 178
    alg: No test for stdrng (krng)
    io scheduler noop registered
    io scheduler deadline registered
    io scheduler cfq registered (default)
    OMAP DSS rev 2.0
    OMAP DISPC rev 3.0
    OMAP VENC rev 2
    OMAP DSI rev 1.0
    Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
    serial8250.0: ttyS0 at MMIO 0x4806a000 (irq = 72) is a ST16654
    console [ttyS0] enabled
    serial8250.1: ttyS1 at MMIO 0x4806c000 (irq = 73) is a ST16654
    serial8250.2: ttyS2 at MMIO 0x49020000 (irq = 74) is a ST16654
    brd: module loaded
    loop: module loaded
    omap2-nand driver initializing
    NAND device: Manufacturer ID: 0x2c, Chip ID: 0xba (Micron NAND 256MiB 1,8V 16-bit)
    Creating 5 MTD partitions on "omap2-nand.0":
    0x000000000000-0x000000080000 : "xloader-nand"
    0x000000080000-0x000000240000 : "uboot-nand"
    0x000000240000-0x000000280000 : "params-nand"
    0x000000280000-0x000000780000 : "linux-nand"
    0x000000780000-0x000010000000 : "jffs2-nand"
    OneNAND driver initializing
    omap2-onenand omap2-onenand: Cannot request GPMC CS
    omap2-onenand: probe of omap2-onenand failed with error -16
    smsc911x: Driver version 2008-10-21.
    smsc911x-mdio: probed
    eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=ffffffff:01, irq=-1)
    net eth0: MAC Address: 00:50:c2:7e:96:fe
    usbcore: registered new interface driver cdc_ether
    usbcore: registered new interface driver dm9601
    ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
    ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
    ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
    ehci-omap ehci-omap.0: irq 77, io mem 0x48064800
    ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
    usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb1: Product: OMAP-EHCI Host Controller
    usb usb1: Manufacturer: Linux 2.6.32 ehci_hcd
    usb usb1: SerialNumber: ehci-omap.0
    hub 1-0:1.0: USB hub found
    hub 1-0:1.0: 3 ports detected
    Initializing USB Mass Storage driver...
    usbcore: registered new interface driver usb-storage
    USB Mass Storage support registered.
    usbcore: registered new interface driver usbtest
    g_ether gadget: using random self ethernet address
    g_ether gadget: using random host ethernet address
    usb0: MAC 0e:3f:e3:cf:00:d1
    usb0: HOST MAC 42:e2:62:42:86:c2
    g_ether gadget: Ethernet Gadget, version: Memorial Day 2008
    g_ether gadget: g_ether ready
    musb_hdrc musb_hdrc: MUSB HDRC host driver
    musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 2
    usb usb2: New USB device found, idVendor=1d6b, idProduct=0002
    usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
    usb usb2: Product: MUSB HDRC host driver
    usb usb2: Manufacturer: Linux 2.6.32 musb-hcd
    usb usb2: SerialNumber: musb_hdrc
    hub 2-0:1.0: USB hub found
    hub 2-0:1.0: 1 port detected
    mice: PS/2 mouse device common for all mice
    input: TWL4030 Keypad as /devices/platform/i2c_omap.1/i2c-1/1-004a/twl4030_keypad/input/input0
    ads7846 spi1.0: touchscreen, irq 335
    input: ADS7846 Touchscreen as /devices/platform/omap2_mcspi.1/spi1.0/input/input1
    twl_rtc twl_rtc: rtc core: registered twl_rtc as rtc0
    twl_rtc twl_rtc: Power up reset detected.
    twl_rtc twl_rtc: Enabling TWL-RTC.
    i2c /dev entries driver
    Linux video capture interface: v2.00
    tvp514x 3-005c: Registered to v4l2 master omap34xxcam!!
    omap-iommu omap-iommu.0: isp: version 1.1
    usbcore: registered new interface driver uvcvideo
    USB Video Class driver (v0.1.0)
    OMAP Watchdog Timer Rev 0x31: initial timeout 60 sec
    usbcore: registered new interface driver usbhid
    usbhid: USB HID core driver
    Advanced Linux Sound Architecture Driver Version 1.0.21.
    usbcore: registered new interface driver snd-usb-audio
    No device for DAI omap-mcbsp-dai-0
    No device for DAI omap-mcbsp-dai-1
    No device for DAI omap-mcbsp-dai-2
    No device for DAI omap-mcbsp-dai-3
    No device for DAI omap-mcbsp-dai-4
    OMAP3 EVM SoC init
    asoc: twl4030 <-> omap-mcbsp-dai-0 mapping ok
    ALSA device list:
    #0: omap3evm (twl4030)
    TCP cubic registered
    NET: Registered protocol family 17
    NET: Registered protocol family 15
    Power Management for TI OMAP3.
    Switched to new clocking rate (Crystal/Core/MPU): 26.0/332/600 MHz
    IVA2 clocking rate: 430 MHz
    SmartReflex driver initialized
    VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 1
    twl_rtc twl_rtc: setting system clock to 2000-01-01 00:00:00 UTC (946684800)
    tvp514x 3-005c: tvp5146m2 found at 0xb8 (OMAP I2C adapter)
    omapdss DPI error: display already enabled
    omap_vout omap_vout: 'lcd' Display already enabled
    omapdss DPI error: display already enabled
    omap_vout omap_vout: 'lcd' Display already enabled
    omap_vout omap_vout: Buffer Size = 3686400
    omap_vout omap_vout: : registered and initialized video device 1
    omap_vout omap_vout: Buffer Size = 3686400
    omap_vout omap_vout: : registered and initialized video device 2
    Waiting for root device /dev/mmcblk0p2...
    mmc0: new high speed SDHC card at address 1234
    mmcblk0: mmc0:1234 SA08G 7.28 GiB
    mmcblk0: p1 p2 p3
    kjournald starting. Commit interval 5 seconds
    EXT3-fs (mmcblk0p2): warning: maximal mount count reached, running e2fsck is recommended
    EXT3-fs (mmcblk0p2): using internal journal
    EXT3-fs (mmcblk0p2): recovery complete
    EXT3-fs (mmcblk0p2): mounted filesystem with writeback data mode
    VFS: Mounted root (ext3 filesystem) on device 179:2.
    Freeing init memory: 172K
    INIT: version 2.86 booting
    Please wait: booting...
    Starting udev
    udev: starting version 141
    udev: renamed network interface eth0 to eth3
    Remounting root file system...
    Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
    ifconfig: SIOCSIFADDR: No such device
    done.
    Setting up IP spoofing protection: rp_filter.
    Thu Jan 13 01:56:00 UTC 2011
    INIT: Entering runlevel: 5
    Starting system message bus: dbus.
    Starting telnet daemon.
    Starting syslogd/klogd: done
    Starting thttpd.
    Starting PVR
    CMEMK module: built on Jan 13 2011 at 00:02:04
    Reference Linux version 2.6.32
    File /sdk/build/DVSDK_4_01/4_01_00_09/arago-install/arago-tmp/work/omap3evm-none-linux-gnueabi/ti-linuxutils-1_2_25_05_11-r91d/linuxutils_2_25_05_11/packages/ti/sdo/c
    allocated heap buffer 0xc7000000 of size 0xf00000
    heap fallback enabled - will try heap if pool buffer is not available
    cmemk initialized
    DSPLINK Module (1.65.00.02) created on Date: Jan 13 2011 Time: 00:05:52
    SDMAK module: built on Jan 13 2011 at 00:02:11
    Reference Linux version 2.6.32
    File /sdk/build/DVSDK_4_01/4_01_00_09/arago-install/arago-tmp/work/omap3evm-none-linux-gnueabi/ti-linuxutils-1_2_25_05_11-r91d/linuxutils_2_25_05_11/packages/ti/sdo/c
    cmemk unregistered
    Setting CMEM Pools to 27MB
    CMEMK module: built on Jan 13 2011 at 00:02:04
    Reference Linux version 2.6.32
    File /sdk/build/DVSDK_4_01/4_01_00_09/arago-install/arago-tmp/work/omap3evm-none-linux-gnueabi/ti-linuxutils-1_2_25_05_11-r91d/linuxutils_2_25_05_11/packages/ti/sdo/c
    allocated heap buffer 0xc9000000 of size 0x6b000
    heap fallback enabled - will try heap if pool buffer is not available
    cmemk initialized
    DSPLINK Module (1.65.00.02) created on Date: Jan 13 2011 Time: 00:05:52
    SDMAK module: built on Jan 13 2011 at 00:02:11
    Reference Linux version 2.6.32
    File /sdk/build/DVSDK_4_01/4_01_00_09/arago-install/arago-tmp/work/omap3evm-none-linux-gnueabi/ti-linuxutils-1_2_25_05_11-r91d/linuxutils_2_25_05_11/packages/ti/sdo/c
    Starting MIDAS
    Drawing UI

    Command is ifconfig eth0:1 192.168.3.202 netmask 255.255.255.0 up
    ifconfig: SIOCSIFADDR: No such device
    Command is udpsvd -v -E 192.168.3.202 69 tftpd /opt/midas &
    SCUOnly is set to false
    SCUOnly is FALSE!
    udpsvd: bind: Cannot assign requested address
    Check in readAPIparams mode params
    Check in readAPIparams valid_bitfield config_all
    Check in readAPIparams inpSatlow 6550
    Check in readAPIparams dBinmed 96
    Check in readAPIparams inpSatmed 15000
    Check in readAPIparams dBinhigh 96
    Check in readAPIparams inpSathigh 65535
    Check in readAPIparams contrast_default high
    Check in readAPIparams contrast_default high
    Check in readAPIparams contrast_default high
    ./userdata/InputData/TI_Carotid_scubparam.txt
    ./userdata/InputData/TI_Carotid_scucparam.txt
    SCUOnly is set to false
    SCUOnly is FALSE!
    Shape is linearCheck in readAPIparams mode params
    Check in readAPIparams valid_bitfield config_all
    Check in readAPIparams inpSatlow 6550
    Check in readAPIparams dBinmed 96
    Check in readAPIparams inpSatmed 15000
    Check in readAPIparams dBinhigh 96
    Check in readAPIparams inpSathigh 65535
    Check in readAPIparams contrast_default high
    Check in readAPIparams contrast_default high
    Check in readAPIparams contrast_default high
    ./userdata/InputData/TI_Carotid_scubparam.txt
    ./userdata/InputData/TI_Carotid_scucparam.txt
    Shape is linearUsFramework_setGlobalMode: Mode set successfully
    getSCUOnly is
    Mode is 3
    dBin is 96
    inpSat is 65535
    0BPU Config NSamplesPerScanLine: 512
    BPU Config Nsamples: 256
    BPU_CONFIG_ALLWallfilter file = ./userdata/LUTs/WALLFilter_TI_Carotid.bin
    *** Note: Wall filter is on
    Opened Color Table File successfully
    In getSCUCparams
    Opened Color Table File successfully
    Opened Arbitration Table File successfully
    WARNING!: Size is 4096 but i is 4096
    Arb over
    UsDisplay_create(): rotation = 0, # buffers = 3

    Block 0: Pool 0: 9 bufs size 4096 (4096 requested)

    Pool 0 busy bufs:
    id 3: phys addr 0x87dfc000 (noncached)
    id 2: phys addr 0x87dfd000 (noncached)
    id 1: phys addr 0x87dfe000 (noncached)
    id 0: phys addr 0x87dff000 (noncached)

    Pool 0 free bufs:
    id 4: phys addr 0x87dfb000
    id 5: phys addr 0x87dfa000
    id 6: phys addr 0x87df9000
    id 7: phys addr 0x87df8000
    id 8: phys addr 0x87df7000

    Block 0: Pool 1: 2 bufs size 131072 (131072 requested)

    Pool 1 busy bufs:
    id 1: phys addr 0x87db7000 (noncached)
    id 0: phys addr 0x87dd7000 (noncached)

    Pool 1 free bufs:

    Block 0: Pool 2: 16 bufs size 524288 (524288 requested)

    Pool 2 busy bufs:

    Pool 2 free bufs:
    id 0: phys addr 0x87d37000
    id 1: phys addr 0x87cb7000
    id 2: phys addr 0x87c37000
    id 3: phys addr 0x87bb7000
    id 4: phys addr 0x87b37000
    id 5: phys addr 0x87ab7000
    id 6: phys addr 0x87a37000
    id 7: phys addr 0x879b7000
    id 8: phys addr 0x87937000
    id 9: phys addr 0x878b7000
    id 10: phys addr 0x87837000
    id 11: phys addr 0x877b7000
    id 12: phys addr 0x87737000
    id 13: phys addr 0x876b7000
    id 14: phys addr 0x87637000
    id 15: phys addr 0x875b7000

    Pool 2 free bufs:

    Block 0: Pool 3: 4 bufs size 131072 (131072 requested)

    Pool 3 busy bufs:
    id 1: phys addr 0x87577000 (noncached)
    id 0: phys addr 0x87597000 (noncached)

    Pool 3 free bufs:
    id 2: phys addr 0x87557000
    id 3: phys addr 0x87537000

    Block 0: Pool 4: 6 bufs size 32768 (32768 requested)

    Pool 4 busy bufs:
    id 5: phys addr 0x87507000 (noncached)
    id 4: phys addr 0x8750f000 (noncached)
    id 3: phys addr 0x87517000 (noncached)
    id 2: phys addr 0x8751f000 (noncached)
    id 1: phys addr 0x87527000 (noncached)
    id 0: phys addr 0x8752f000 (noncached)

    Pool 4 free bufs:

    Block 0: Pool 5: 2 bufs size 16384 (16384 requested)

    Pool 5 busy bufs:

    Pool 5 free bufs:
    id 0: phys addr 0x87503000
    id 1: phys addr 0x874ff000

    Block 0: Pool 6: 8 bufs size 1843200 (1843200 requested)

    Pool 6 busy bufs:

    Pool 6 free bufs:
    id 0: phys addr 0x8733d000
    id 1: phys addr 0x8717b000
    id 2: phys addr 0x86fb9000
    id 3: phys addr 0x86df7000
    id 4: phys addr 0x86c35000
    id 5: phys addr 0x86a73000
    id 6: phys addr 0x868b1000
    id 7: phys addr 0x866ef000

    Block 0: Pool 7: 4 bufs size 921600 (921600 requested)

    Pool 7 busy bufs:

    Pool 7 free bufs:
    id 0: phys addr 0x8660e000
    id 1: phys addr 0x8652d000
    id 2: phys addr 0x8644c000
    id 3: phys addr 0x8636b000
    hUsProcess:SCUOnly is 0BEFORE DPUBUFTABOUT16 CREATE

    Block 0: Pool 0: 9 bufs size 4096 (4096 requested)

    Pool 0 busy bufs:
    id 3: phys addr 0x87dfc000 (noncached)
    id 2: phys addr 0x87dfd000 (noncached)
    id 1: phys addr 0x87dfe000 (noncached)
    id 0: phys addr 0x87dff000 (noncached)

    Pool 0 free bufs:
    id 4: phys addr 0x87dfb000
    id 5: phys addr 0x87dfa000
    id 6: phys addr 0x87df9000
    id 7: phys addr 0x87df8000
    id 8: phys addr 0x87df7000

    Block 0: Pool 1: 2 bufs size 131072 (131072 requested)

    Pool 1 busy bufs:
    id 1: phys addr 0x87db7000 (noncached)
    id 0: phys addr 0x87dd7000 (noncached)

    Pool 1 free bufs:

    Block 0: Pool 2: 16 bufs size 524288 (524288 requested)

    Pool 2 busy bufs:

    Pool 2 free bufs:
    id 0: phys addr 0x87d37000
    id 1: phys addr 0x87cb7000
    id 2: phys addr 0x87c37000
    id 3: phys addr 0x87bb7000
    id 4: phys addr 0x87b37000
    id 5: phys addr 0x87ab7000
    id 6: phys addr 0x87a37000
    id 7: phys addr 0x879b7000
    id 8: phys addr 0x87937000
    id 9: phys addr 0x878b7000
    id 10: phys addr 0x87837000
    id 11: phys addr 0x877b7000
    id 12: phys addr 0x87737000
    id 13: phys addr 0x876b7000
    id 14: phys addr 0x87637000
    id 15: phys addr 0x875b7000

    Pool 2 free bufs:

    Block 0: Pool 3: 4 bufs size 131072 (131072 requested)

    Pool 3 busy bufs:
    id 3: phys addr 0x87537000 (noncached)
    id 2: phys addr 0x87557000 (noncached)
    id 1: phys addr 0x87577000 (noncached)
    id 0: phys addr 0x87597000 (noncached)

    Pool 3 free bufs:

    Block 0: Pool 4: 6 bufs size 32768 (32768 requested)

    Pool 4 busy bufs:
    id 5: phys addr 0x87507000 (noncached)
    id 4: phys addr 0x8750f000 (noncached)
    id 3: phys addr 0x87517000 (noncached)
    id 2: phys addr 0x8751f000 (noncached)
    id 1: phys addr 0x87527000 (noncached)
    id 0: phys addr 0x8752f000 (noncached)

    Pool 4 free bufs:

    Block 0: Pool 5: 2 bufs size 16384 (16384 requested)

    Pool 5 busy bufs:

    Pool 5 free bufs:
    id 0: phys addr 0x87503000
    id 1: phys addr 0x874ff000

    Block 0: Pool 6: 8 bufs size 1843200 (1843200 requested)

    Pool 6 busy bufs:

    Pool 6 free bufs:
    id 0: phys addr 0x8733d000
    id 1: phys addr 0x8717b000
    id 2: phys addr 0x86fb9000
    id 3: phys addr 0x86df7000
    id 4: phys addr 0x86c35000
    id 5: phys addr 0x86a73000
    id 6: phys addr 0x868b1000
    id 7: phys addr 0x866ef000

    Block 0: Pool 7: 4 bufs size 921600 (921600 requested)

    Pool 7 busy bufs:

    Pool 7 free bufs:
    id 0: phys addr 0x8660e000
    id 1: phys addr 0x8652d000
    id 2: phys addr 0x8644c000
    id 3: phys addr 0x8636b000
    BEFORE DPUBUFTABOUT8 CREATE

    Block 0: Pool 0: 9 bufs size 4096 (4096 requested)

    Pool 0 busy bufs:
    id 3: phys addr 0x87dfc000 (noncached)
    id 2: phys addr 0x87dfd000 (noncached)
    id 1: phys addr 0x87dfe000 (noncached)
    id 0: phys addr 0x87dff000 (noncached)

    Pool 0 free bufs:
    id 4: phys addr 0x87dfb000
    id 5: phys addr 0x87dfa000
    id 6: phys addr 0x87df9000
    id 7: phys addr 0x87df8000
    id 8: phys addr 0x87df7000

    Block 0: Pool 1: 2 bufs size 131072 (131072 requested)

    Pool 1 busy bufs:
    id 1: phys addr 0x87db7000 (noncached)
    id 0: phys addr 0x87dd7000 (noncached)

    Pool 1 free bufs:

    Block 0: Pool 2: 16 bufs size 524288 (524288 requested)

    Pool 2 busy bufs:
    id 1: phys addr 0x87cb7000 (noncached)
    id 0: phys addr 0x87d37000 (noncached)

    Pool 1 free bufs:

    Pool 2 free bufs:
    id 2: phys addr 0x87c37000
    id 3: phys addr 0x87bb7000
    id 4: phys addr 0x87b37000
    id 5: phys addr 0x87ab7000
    id 6: phys addr 0x87a37000
    id 7: phys addr 0x879b7000
    id 8: phys addr 0x87937000
    id 9: phys addr 0x878b7000
    id 10: phys addr 0x87837000
    id 11: phys addr 0x877b7000
    id 12: phys addr 0x87737000
    id 13: phys addr 0x876b7000
    id 14: phys addr 0x87637000
    id 15: phys addr 0x875b7000

    Pool 2 free bufs:

    Block 0: Pool 3: 4 bufs size 131072 (131072 requested)

    Pool 3 busy bufs:
    id 3: phys addr 0x87537000 (noncached)
    id 2: phys addr 0x87557000 (noncached)
    id 1: phys addr 0x87577000 (noncached)
    id 0: phys addr 0x87597000 (noncached)

    Pool 3 free bufs:

    Block 0: Pool 4: 6 bufs size 32768 (32768 requested)

    Pool 4 busy bufs:
    id 5: phys addr 0x87507000 (noncached)
    id 4: phys addr 0x8750f000 (noncached)
    id 3: phys addr 0x87517000 (noncached)
    id 2: phys addr 0x8751f000 (noncached)
    id 1: phys addr 0x87527000 (noncached)
    id 0: phys addr 0x8752f000 (noncached)

    Pool 4 free bufs:

    Block 0: Pool 5: 2 bufs size 16384 (16384 requested)

    Pool 5 busy bufs:

    Pool 5 free bufs:
    id 0: phys addr 0x87503000
    id 1: phys addr 0x874ff000

    Block 0: Pool 6: 8 bufs size 1843200 (1843200 requested)

    Pool 6 busy bufs:

    Pool 6 free bufs:
    id 0: phys addr 0x8733d000
    id 1: phys addr 0x8717b000
    id 2: phys addr 0x86fb9000
    id 3: phys addr 0x86df7000
    id 4: phys addr 0x86c35000
    id 5: phys addr 0x86a73000
    id 6: phys addr 0x868b1000
    id 7: phys addr 0x866ef000

    Block 0: Pool 7: 4 bufs size 921600 (921600 requested)

    Pool 7 busy bufs:

    Pool 7 free bufs:
    id 0: phys addr 0x8660e000
    id 1: phys addr 0x8652d000
    id 2: phys addr 0x8644c000
    id 3: phys addr 0x8636b000
    BEFORE SCUBUFTABOUT16 CREATE
    UsProcess: CMEM allocation of 7372800 bytes for hSCUBufTabOut16

    Block 0: Pool 0: 9 bufs size 4096 (4096 requested)

    Pool 0 busy bufs:
    id 3: phys addr 0x87dfc000 (noncached)
    id 2: phys addr 0x87dfd000 (noncached)
    id 1: phys addr 0x87dfe000 (noncached)
    id 0: phys addr 0x87dff000 (noncached)

    Pool 0 free bufs:
    id 4: phys addr 0x87dfb000
    id 5: phys addr 0x87dfa000
    id 6: phys addr 0x87df9000
    id 7: phys addr 0x87df8000
    id 8: phys addr 0x87df7000

    Block 0: Pool 1: 2 bufs size 131072 (131072 requested)

    Pool 1 busy bufs:
    id 1: phys addr 0x87db7000 (noncached)
    id 0: phys addr 0x87dd7000 (noncached)

    Pool 1 free bufs:

    Block 0: Pool 2: 16 bufs size 524288 (524288 requested)

    Pool 2 busy bufs:
    id 1: phys addr 0x87cb7000 (noncached)
    id 0: phys addr 0x87d37000 (noncached)

    Pool 1 free bufs:

    Pool 2 free bufs:
    id 2: phys addr 0x87c37000
    id 3: phys addr 0x87bb7000
    id 4: phys addr 0x87b37000
    id 5: phys addr 0x87ab7000
    id 6: phys addr 0x87a37000
    id 7: phys addr 0x879b7000
    id 8: phys addr 0x87937000
    id 9: phys addr 0x878b7000
    id 10: phys addr 0x87837000
    id 11: phys addr 0x877b7000
    id 12: phys addr 0x87737000
    id 13: phys addr 0x876b7000
    id 14: phys addr 0x87637000
    id 15: phys addr 0x875b7000

    Pool 2 free bufs:

    Block 0: Pool 3: 4 bufs size 131072 (131072 requested)

    Pool 3 busy bufs:
    id 3: phys addr 0x87537000 (noncached)
    id 2: phys addr 0x87557000 (noncached)
    id 1: phys addr 0x87577000 (noncached)
    id 0: phys addr 0x87597000 (noncached)

    Pool 3 free bufs:

    Block 0: Pool 4: 6 bufs size 32768 (32768 requested)

    Pool 4 busy bufs:
    id 5: phys addr 0x87507000 (noncached)
    id 4: phys addr 0x8750f000 (noncached)
    id 3: phys addr 0x87517000 (noncached)
    id 2: phys addr 0x8751f000 (noncached)
    id 1: phys addr 0x87527000 (noncached)
    id 0: phys addr 0x8752f000 (noncached)

    Pool 4 free bufs:

    Block 0: Pool 5: 2 bufs size 16384 (16384 requested)

    Pool 5 busy bufs:

    Pool 5 free bufs:
    id 0: phys addr 0x87503000
    id 1: phys addr 0x874ff000

    Pool 5 free bufs:

    Block 0: Pool 6: 8 bufs size 1843200 (1843200 requested)

    Pool 6 busy bufs:
    id 3: phys addr 0x86df7000 (noncached)
    id 2: phys addr 0x86fb9000 (noncached)
    id 1: phys addr 0x8717b000 (noncached)
    id 0: phys addr 0x8733d000 (noncached)

    Pool 6 free bufs:
    id 4: phys addr 0x86c35000
    id 5: phys addr 0x86a73000
    id 6: phys addr 0x868b1000
    id 7: phys addr 0x866ef000

    Block 0: Pool 7: 4 bufs size 921600 (921600 requested)

    Pool 7 busy bufs:

    Pool 7 free bufs:
    id 0: phys addr 0x8660e000
    id 1: phys addr 0x8652d000
    id 2: phys addr 0x8644c000
    id 3: phys addr 0x8636b000
    BEFORE SCUBUFTABOUT8 CREATE
    UsProcess: CMEM allocation of 3686400 bytes for hSCUBufTabOut8
    PROFILE_DEMO: Profile info available on console
    PROFILE_DEMO: DDRALGHEAP memory takes 15411320 bytes
    Initializing Process Thread
    Entering UsControl Thread
    Allocation Complete
    6472 Booted Successfully
    tcpsendconnect: Network is unreachable
    can't send wild card teardown
    tcpsendconnect: Network is unreachable
    ERROR: Failed rdspc_setup
    Carotid Data to tmp (DDR) successful
    Carotid Data to tmp (DDR) successful
    Imaging started
    dBin is 96
    inpSat is 65535
    BPU Config NSamplesPerScanLine: 512
    BPU Config Nsamples: 256
    BPU_CONFIG_ALLWallfilter file = ./userdata/LUTs/WALLFilter_TI_Carotid.bin
    *** Note: Wall filter is on
    Opened Color Table File successfully
    In getSCUCparams
    Opened Color Table File successfully
    Opened Arbitration Table File successfully
    WARNING!: Size is 4096 but i is 4096
    Arb over
    Before BPU Config
    UsProcess_configBpu: App-> Control completed
    After BPU Config
    UsProcess_configDpu: Configuration before DSP send: sz=2078 bytes nscan=48
    UsProcess_configDpu: App-> Control completed
    UsProcess_configScuB: Configuration before DSP send: inlines=256, insamples=512, outrows=1280, outcols=720
    SCU mode=bmode
    UsProcess_configScuB: App-> Control completed
    Color Configuration before DSP send: inlines=48, insamples=256, outrows=1280, outcols=720
    UsProcess_configScuColor:App->Control completed.
    Check Input file B is "./userdata/InputData/TI_Carotid_tissdata_512x256x69.bin"
    Check Input file C is "/tmp/TI_Carotid_velturbdata_48x256x10x69.bin"
    InputFrame Size B is 524288
    InputFrame Size Color is 491520
    Check SCUOnly is false
    Acquire Thread Initialized
    UsAcquire_init completed
    Creating Acquire ThreadStarting Acquire Thread
    Starting Display thread
    Rendezvous Met
    Starting Process Thread
    6472 Unavailable. Using Input Files
    PROFILE_DEMO: Time for Check Header = 47638 us per frame
    PROFILE_DEMO: Time for Fifo Get = 214 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 30 us per frame
    PROFILE_DEMO: Time for BPU = 5921 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 26520 us per frame
    PROFILE_DEMO: Time for DPU = 5402 us per frame
    PROFILE_DEMO: Time for SCU Color = 33570 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 30 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 26429 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 6103 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33753 us per frame
    PROFILE_DEMO: Time for Acquire = 183 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 20324 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 6012 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33600 us per frame
    PROFILE_DEMO: Time for Acquire = 183 us per frame
    PROFILE_DEMO: Time for Check Header = 48706 us per frame
    PROFILE_DEMO: Time for Fifo Get = 8392 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 92 us per frame
    PROFILE_DEMO: Time for BPU = 5737 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 27191 us per frame
    PROFILE_DEMO: Time for DPU = 5249 us per frame
    PROFILE_DEMO: Time for SCU Color = 32898 us per frame
    PROFILE_DEMO: DSP Load is 47%
    PROFILE_DEMO: ARM Load is 97%
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 214 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4730 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33722 us per frame
    PROFILE_DEMO: Time for Acquire = 153 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 183 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4852 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33722 us per frame
    PROFILE_DEMO: Time for Acquire = 122 us per frame
    PROFILE_DEMO: Time for Check Header = 47455 us per frame
    PROFILE_DEMO: Time for Fifo Get = 7385 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 61 us per frame
    PROFILE_DEMO: Time for BPU = 5768 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 25849 us per frame
    PROFILE_DEMO: Time for DPU = 5279 us per frame
    PROFILE_DEMO: Time for SCU Color = 32807 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 123 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4760 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33722 us per frame
    PROFILE_DEMO: Time for Acquire = 153 us per frame
    PROFILE_DEMO: DSP Load is 54%
    PROFILE_DEMO: ARM Load is 100%
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 153 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4791 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33722 us per frame
    PROFILE_DEMO: Time for Acquire = 152 us per frame
    PROFILE_DEMO: Time for Check Header = 47791 us per frame
    PROFILE_DEMO: Time for Fifo Get = 214 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 30 us per frame
    PROFILE_DEMO: Time for BPU = 5798 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 19989 us per frame
    PROFILE_DEMO: Time for DPU = 5402 us per frame
    PROFILE_DEMO: Time for SCU Color = 32654 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 153 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 3875 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33631 us per frame
    PROFILE_DEMO: Time for Acquire = 122 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 122 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4730 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33722 us per frame
    PROFILE_DEMO: Time for Acquire = 122 us per frame
    PROFILE_DEMO: Time for Check Header = 46845 us per frame
    PROFILE_DEMO: Time for Fifo Get = 213 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 31 us per frame
    PROFILE_DEMO: Time for BPU = 5768 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 25421 us per frame
    PROFILE_DEMO: Time for DPU = 5219 us per frame
    PROFILE_DEMO: Time for SCU Color = 34272 us per frame
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 122 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 3845 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33661 us per frame
    PROFILE_DEMO: Time for Acquire = 152 us per frame
    PROFILE_DEMO: DSP Load is 55%
    PROFILE_DEMO: ARM Load is 100%
    PROFILE_DEMO: Time for Acquire 1 = 0 us per frame
    PROFILE_DEMO: Time for Acquire 2 = 122 us per frame
    PROFILE_DEMO: Time for Acquire 3 = 4670 us per frame
    PROFILE_DEMO: Time for Acquire 4 = 33569 us per frame
    PROFILE_DEMO: Time for Acquire = 153 us per frame
    PROFILE_DEMO: Time for Check Header = 47851 us per frame
    PROFILE_DEMO: Time for Fifo Get = 153 us per frame
    PROFILE_DEMO: Time for Check Header n Fifo Get = 30 us per frame
    PROFILE_DEMO: Time for BPU = 4914 us per frame
    PROFILE_DEMO: Time for SCU (Bmode) = 25787 us per frame
    PROFILE_DEMO: Time for DPU = 5280 us per frame

    I could not find ultrasound -qws in the etc/init.d/rcS so i could not try ping. It had

    #!/bin/sh
    #
    # rcS Call all S??* scripts in /etc/rcS.d in
    # numerical/alphabetical order.
    #
    # Version: @(#)/etc/init.d/rcS 2.76 19-Apr-1999 miquels@cistron.nl
    #

    PATH=/sbin:/bin:/usr/sbin:/usr/bin
    runlevel=S
    prevlevel=N
    umask 022
    export PATH runlevel prevlevel

    # Make sure proc is mounted
    #
    [ -d "/proc/1" ] || mount /proc

    #
    # See if system needs to be setup. This is ONLY meant to
    # be used for the initial setup after a fresh installation!
    #
    if [ -x /sbin/unconfigured.sh ]
    then
    /sbin/unconfigured.sh
    fi

    #
    # Source defaults.
    #
    . /etc/default/rcS

    #
    # Trap CTRL-C &c only in this shell so we can interrupt subprocesses.
    #
    trap ":" INT QUIT TSTP

    #
    # Call all parts in order.
    #
    exec /etc/init.d/rc S

    #
    # For compatibility, run the files in /etc/rc.boot too.
    #
    [ -d /etc/rc.boot ] && run-parts /etc/rc.boot

    #
    # Finish setup if needed. The comment above about
    # /sbin/unconfigured.sh applies here as well!
    #
    if [ -x /sbin/setup.sh ]
    then
    /sbin/setup.sh
    fi

    Thanks

  • Hi uday or someone

    I am able to ping my omap3530 with proxy 192.168.3.205 but unable to ping my C6678 after executing the .out files from midas ultrasound v4.0. can anyone help me out?

    Thanks

  • Hi Vivek

    From your log I see the following error condition:

    "Configuring network interfaces... ifconfig: SIOCGIFFLAGS: No such device
    ifconfig: SIOCSIFADDR: No such device

    Command is ifconfig eth0:1 192.168.3.202 netmask 255.255.255.0 up 
    ifconfig: SIOCSIFADDR: No such device" 

    And the reason seems to be the following in your log, which says:

    "udev: starting version 141
    udev: renamed network interface eth0 to eth3"

    The MIDAS code in the SD card assumes eth0. Your OMAP EVM for some reason is not able to configure the network interface to eth0 and uses eth3 instead. 

    So let's do this. Comment out ./ultrasound -qws from your init.d/rcS script so that the ultrasound executable doesn't auto-start on boot. Now when the OMAP completes booting, you should see the linux command prompt. Execute the following command:

    ifconfig eth3:1 192.168.3.202 netmask 255.255.255.0 up

    Then run the ultrasound demo executable as 

    ./ultrasound -qws

    Hopefully this addresses the issue. If not, please reply with a new log.