This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm6446 hangs

hi,

please provide solution for this, dm446evm hangs once itstart booting kernel, below is the details,

--------------------------------------------


U-Boot 1.1.3 (Dec  4 2006 - 12:05:38)

U-Boot code: 81080000 -> 81097628  BSS: -> 810A0018
RAM Configuration:
Bank #0: 80000000 256 MB
Flash: 16 MB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 297MHz
DDR Clock :- 162MHz
Hit any key to stop autoboot:  0
## Booting image at 02050000 ...
   Image Name:   Linux-2.6.10_mvl401-davinci_evm
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1333196 Bytes =  1.3 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
OK

Starting kernel ...

Uncompressing Linux.............................................................
Linux version 2.6.10_mvl401-davinci_evm (xlibrary@scarletoak.sanb.design.ti.com)
 (gcc version 3.4.3 (MontaVista 3.4.3-25.0.30.0501131 2005-07-23)) #2 Mon Aug 7
14:58:21 PDT 2006
CPU: ARM926EJ-Sid(wb) [41069265] revision 5 (ARMv5TEJ)
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Machine: DaVinci EVM
Memory policy: ECC disabled, Data cache writeback
Built 1 zonelists
Kernel command line: console=ttyS0,115200n8 noinitrd rw ip=dhcp root=/dev/nfs nf
sroot=127.0.0.1:, nolock mem=120M
PID hash table entries: 512 (order: 9, 8192 bytes)
Console: colour dummy device 80x30
Dentry cache hash table entries: 16384 (order: 4, 65536 bytes)
Inode-cache hash table entries: 8192 (order: 3, 32768 bytes)
Memory: 120MB = 120MB total
Memory: 118784KB available (2271K code, 480K data, 136K init)
Mount-cache hash table entries: 512 (order: 0, 4096 bytes)
CPU: Testing write buffer coherency: ok
spawn_desched_task(00000000)
desched cpu_callback 3/00000000
ksoftirqd started up.
desched cpu_callback 2/00000000
desched thread 0 started up.
NET: Registered protocol family 16
Registering platform device 'musb_hdrc'. Parent at platform
DaVinci I2C DEBUG: 12:15:02 Aug  1 2006
Registering platform device 'i2c'. Parent at platform
usbcore: registered new driver usbfs
usbcore: registered new driver hub
JFFS2 version 2.2. (NAND) (C) 2001-2003 Red Hat, Inc.
yaffs Aug  1 2006 12:14:38 Installing.
Registering platform device 'davincifb.0'. Parent at platform
Setting Up Clocks for DM420 OSD
Console: switching to colour frame buffer device 90x30
fb0: dm_osd0_fb frame buffer device
fb1: dm_vid0_fb frame buffer device
fb2: dm_osd1_fb frame buffer device
fb3: dm_vid1_fb frame buffer device
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
Registering platform device 'serial8250'. Parent at platform
ttyS0 at MMIO 0x1c20000 (irq = 40) is a 16550A
io scheduler noop registered
io scheduler anticipatory registered
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Registering platform device 'ti_davinci_emac'. Parent at platform
TI DaVinci EMAC: MAC address is 00:0e:99:02:5a:1a
TI DaVinci EMAC Linux version updated 4.0
TI DaVinci EMAC: Installed 1 instances.
netconsole: not configured, aborting
i2c /dev entries driver
Linux video capture interface: v1.00
Registering platform device 'vpfe.1'. Parent at platform
DaVinci v4l2 capture driver V1.0 loaded
Uniform Multi-Platform E-IDE driver Revision: 7.00alpha2
ide: Assuming 50MHz system bus speed for PIO modes; override with idebus=xx
hda: TOSHIBA MK4032GAX, ATA DISK drive
elevator: using anticipatory as default io scheduler
ide0 at 0xe10661f0-0xe10661f7,0xe10663f6 on irq 22
hda: max request size: 1024KiB
hda: 78140160 sectors (40007 MB), CHS=16383/255/63
 hda: hda1 hda2
    ide0: BM-DMA at 0xe1066000-0xe1066007, BIOS settings: hda:pio, hdb:pio
mice: PS/2 mouse device common for all mice
musb_hdrc: version 2.2a/db-0.4.8 [pio] [host] [debug=0]
musb_hdrc: USB Host mode controller at c8060000 using PIO, IRQ 12
musb_hdrc musb_hdrc: new USB bus registered, assigned bus number 1
hub 1-0:1.0: USB hub found
hub 1-0:1.0: 1 port detected
Registering platform device 'davinci-audio.0'. Parent at platform
NET: Registered protocol family 2
IP: routing cache hash table of 512 buckets, 4Kbytes
TCP: Hash tables configured (established 8192 bind 16384)
NET: Registered protocol family 1
NET: Registered protocol family 17
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)...
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)...
Sending DHCP requests ...... timed out!
IP-Config: Retrying forever (NFS root)...
Sending DHCP requests ....

it will hang here.. can you provide me the initial setup env, that i can start fresh..