This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Client-Server Application with C6670 and a PC

Hello all,

I want to establish a connection between a C6670 and a PC where the C6670 sends a request to the PC, the app on the PC does some operations and sends back the result. I intend to do the APP on the PC with C/C++ and use Winsock for communication with the C6670. Does anyone has some experience with a routine like this? The reason by the way why I chose C/C++ for app on the PC is that I need fast calculations using log operations. Further this process should have a constant response time as it is for time-critical application. So, where can I start? Is there any example code for connection between a C6670 and PC?

Best regards,

Burak