How to check whether new data is available in Rx register ,when SPI master is in receive only mode?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
How to check whether new data is available in Rx register ,when SPI master is in receive only mode?
Hi Sujith,
In the master receive-only mode, software must write dummy data to the MCSPI_TXx register, and only after the TX buffer is empty (check the MCSPI_CH0STAT[2] bit in the software). Only one dummy write is enough to receive any number of words from the slave. Software should ensure that the MCSPI_TXx register is always full (the TXx_EMPTY bits of SPIm.MCSPI_IRQSTATUS) when receiving. The content of the MCSPI_TXx register is always loaded into the shift register when the shift register is assigned. After writing the dummy data to the MCSPI_TXx register, the TXx_EMPTY and TXx_UNDERFLOW bits in the SPIm.MCSPI_IRQSTATUS register are never set in receive-only mode.
For more details refer to TRM section 20.5.2.4 Master Receive-Only Mode (Half Duplex)
http://www.ti.com/lit/ug/sprugn4r/sprugn4r.pdf
BR
Tsvetolin Shulev
HI Cvetolin,
I need a clarity on this statement "Software should ensure that the MCSPI_TXx register is always full (the TXx_EMPTY bits of SPIm.MCSPI_IRQSTATUS) when receiving".
I am not enabling Interrupt , I am using polling method for status check. When i continuously check the status bit i observe that The RXS bit in the Status register is always full and TXS register is always empty .
When i try to read the Receive register based on the RXS bit full condition,I seen that Receive register is not updated.