Dear TI experts,
I'm at the decision making stage of a system equipped with C6670 and an IF transceiver channel.
I need the C6670 to provide a ~100 kHz clock (TTL) which should be strictly synchronized with the IF transceiver which is operated with 600 MHz clock. While I can use the IF transceiver clock (am I, what is the maximal frequency?) as an external clock on timer input, I couldn't find the means to synchronize the timer with SYNC signal from the transceiver.
Could someone drop me a hint on how to do that?
Thank you in advance, Alon.