This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel doesn't support SATA HD larger than 3TB

Hi,

My customer report the Kernel in DVR-RDK 3.5 doesn't support SATA HD large as 3TB. Is there any updates on the kernel can support this feature?

Below is their log:

ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300)

ata1.15: Port Multiplier 1.2, 0x197b:0x3215 r0, 5 ports, feat 0x5/0xf

ata1.00: hard resetting link

ata1.00: SATA link down (SStatus 0 SControl 320)

ata1.01: hard resetting link

ata1.01: SATA link up 3.0 Gbps (SStatus 123 SControl 320)

ata1.02: hard resetting link

ata1.02: SATA link down (SStatus 0 SControl 320)

ata1.03: hard resetting link

ata1.03: SATA link down (SStatus 0 SControl 320)

ata1.04: hard resetting link

ata1.04: SATA link down (SStatus 0 SControl 320)

ata1.01: ATA-8: ST3000VX000-1CU166, CV22, max UDMA/133

ata1.01: 5860533168 sectors, multi 0: LBA48 NCQ (depth 31/32)

ata1.01: configured for UDMA/133

ata1: EH complete

scsi 0:1:0:0: Direct-Access     ATA      ST3000VX000-1CU1 CV22 PQ: 0 ANSI: 5

sd 0:1:0:0: Attached scsi generic sg0 type 0

sd 0:1:0:0: [sda] Too big for this kernel. Use a kernel compiled with support for large block devices.

sd 0:1:0:0: [sda] Unsupported sector size -75.

sd 0:1:0:0: [sda] 0 512-byte logical blocks: (0 B/0 B)

sd 0:1:0:0: [sda] 0-byte physical blocks

sd 0:1:0:0: [sda] Write Protect is off

sd 0:1:0:0: [sda] Write cache: enabled, read cache: enabled, doesn't support DPO or FUA

sd 0:1:0:0: [sda] Too big for this kernel. Use a kernel compiled with support for large block devices.

sd 0:1:0:0: [sda] Unsupported sector size -75.

sd 0:1:0:0: [sda] Attached SCSI disk

BR,

Eason