This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ICE Board AM3359 : Ethercat application

Hi,

We have two ICE  slave boards from TI,

Example

Salve 1 : Only configured with Digital input

Slave 2: Configured with Digital output

Note :- we have configured the XML file and code occordingly, and found to be working independently with Twincat

When we connect both the slave board and tried to communicate through twincat : communication is not done

Can any one please guide :

1) How the 2 slaves are differenciated

2) should some change need to be done in XML ( to differentiate slaves).

3) should some change need to done in code (to differentiate slaves).

Thanks,

Bindu

  • Hi Bindu,

    This does not appear to be a BIOS question.

    Are you working with a particular SDK?

    If you provide some more information on the software product you're using (and or having problems with), we will be able to get your question to the appropriate team that can help you.

    Steve