Other Parts Discussed in Thread: AM3359
Hi,
We are using the ecat_appl example.
SPI 1 Module is provided with
API used : McSPIClkConfig
SPI in Clock : spiInClk ( 48 MHZ)
SPI out clock : spiOutClk ,
Can any one please guide on below points as we are connecting a slave which could be configured upto 30MHZ
AM3359 is master mode
1) What is the maximum spiOutClk that can be generated on SPI line
2) Can we change the spiInClk to increase the spiOutClk
Thanks,
Bindu