This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Regarding suggestion for board

Dear sir/madam,

I am planning do a project on DSP, In that project i want process both image and audio simultaneously , below i have mentioned brief explanation about my project please suggest me a proper hardware which suits for it.

In my project i want to give a image as input from scanner and same time i want to give the some wave files through audio jack after processing these signal , i want to see that processed image on display and simultaneously i want to listen that audio through the audio jack .

This is brief idea about my project please suggest me proper hardware which suits this applicatoin

i thought to do this using DM6437/DM642 but i think there is no facility to give input from scanner on that board. 

Please suggest a device 

  • Pyati,

    You've not given the details of the interface through which you are going to input the image data to the SoC. But anyways, DM365 will be a very good platform for your use case. You can purchase DM365 EVM from Spectrum Digital as well. It can handle audio as well.