Hi all,
I want to use the Dallas 1-Wire port for accessing the DS2781 battery monitor chip. I use my own OMAP4 board running the kernel 3.4 included in the package 4AJ.2.5 from omappedia. I assume I need at least the OMAP 1-wire master and the DS2781 slave driver.
How can I enable the 1-Wire master driver for OMAP4?
The existing define CONFIG_HDQ_MASTER_OMAP can only be set for the SOC_OMAP2430 or the ARCH_OMAP3 architecture.
Does there exist a patch for kernel 3.4 (used in 4AJ.2.5) or can I use the existing omap_hdq.c also for OMAP4?
Best regards,
Roman