This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LRW datagram on IGH and 335x ICE development kit 10.0.0.8

Other Parts Discussed in Thread: AM3359, SYSBIOS

Hi all,

I've a problem in FMMU configuration on the ecat_appl example of AM3359 ICE development kit.

I've captured with wireshark the ethercat data from the IGH master and ICE, the SM is used with Freerun configuration.

https://dl.dropboxusercontent.com/u/91173447/wireshark_igh_ti_ice.pcapng

The problem is that IGH doesn't make an optimization of FMMU using LRW datagram; using twincat (that works) the FMMU are configured to save space on datagram (so the LRW has just 7 bytes data not 7+5 bytes as IGH).

Although could be better make this optimization, (I've cheched that this is the problem making a software patch on master and the working counter goes to the desired value of 3), I was wondering is this behaviour of ESC is wrong and can be modified.