Other Parts Discussed in Thread: AM3352
hi all
I use am3352 cpu. Now, Spi operate with edma3
I Want to be SPI TX Edma Completion Interrupt occurs.
However, 'Edma Complete Interrupt ' faster than 'Transfer complte' occurs.
My configurations
1. MMU Enable, ICACHE and DACAHE Enable.
2. paramSet.srcAddr = (unsigned int) buffer;
paramSet.destAddr = (unsigned int) (MCSPI0_TX(1));
paramSet.aCnt = 1;
paramSet.bCnt = buffLength;
paramSet.cCnt = 1;
paramSet.srcBIdx = 1; paramSet.destBIdx = 0;
paramSet.srcCIdx = 0; paramSet.destCIdx = 0;
paramSet.linkAddr = (EDMA3CC_OPT(DUMMY_CH_NUM)); paramSet.bCntReload = 0;
paramSet.opt = 0x00000000;
paramSet.opt |= ((tccNum << EDMA3CC_OPT_TCC_SHIFT) & EDMA3CC_OPT_TCC);
paramSet.opt |= (1 << EDMA3CC_OPT_TCINTEN_SHIFT);
EDMA3SetPaRAM(SOC_EDMA30CC_0_REGS, chNum, ¶mSet);
TxDummyPaRAMConfEnable();
EDMA3EnableTransfer(SOC_EDMA30CC_0_REGS, chNum, EDMA3_TRIG_MODE_EVENT);
3 . SPI SINGLE CHANNEL, MASTER TX ONLY, 6MHZ, Setting
4. Enable SPIDMA
5. after tx complete, In Compete ISR , Wait IPR or IPRH Setting
6. Clear Interrupt Flag, Disable SPI DMA
spi_clk _-_-_-_-_-_-_-_-_-_________
tx ___--___-___--_-_________ (TX Complete)
Interrupt complete -------------------_______-------- (GPIO Low Output in Edma Complete ISR)
14bytes 32bytes
If SPI transfer 32bytes , Ideally, the interrupt must occur after the transfer 32bytes
However, interrupt is generated after 14bytes transfer.
After interrupt occurs , clock and the data is lost
What is the problem?
Thanks.