Other Parts Discussed in Thread: TMS320C5515
Hello,
I am working with CCSv4 and TMS320C5515. I developed a program and generate the binary file. I downloaded EVM_5515_programmer.out and I used it to load the bin file into memory. I downloaded it to NOR flash and NAND flash with no problem, However, when I try to download it to SPI EEPROM or I2C EEPROM, I get this error:
Writing data to device...
Opening C:\projecte1\Debug\projecte1.bin...
Input file opened
WRITE ERROR! at 0x00000000
Wrote 0x0000 Read 0x09aa
Also, I want to ask if there are any executable or application to load binary files to eeprom without using code composer studio.
I hope you can help me please! Thank you