This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335x GPMC with FPGA



I can use GPMC to write any data to FPGA, but I just could read 0 from FPGA under CE.

The same operation in starterware is OK.

Please help me to clarifiy the problem.

Here is my setting in wince:


void GPMCPinMuxSetup(void)
{
    /* GPMC_AD0 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(0), 0x30);

    /* GPMC_AD1 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(1), 0x30);

    /* GPMC_AD2 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(2), 0x30);

    /* GPMC_AD3 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(3), 0x30);

    /* GPMC_AD4 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(4), 0x30);

    /* GPMC_AD5 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(5), 0x30);

    /* GPMC_AD6 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(6), 0x30);

    /* GPMC_AD7 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(7), 0x30);

    /* GPMC_AD8 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(8), 0x30);

    /* GPMC_AD9 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(9), 0x30);

    /* GPMC_AD10 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(10), 0x30);

    /* GPMC_AD11 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(11), 0x30);

    /* GPMC_AD12 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(12), 0x30);

    /* GPMC_AD13 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(13), 0x30);

    /* GPMC_AD14 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(14), 0x30);

    /* GPMC_AD15 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_AD(15), 0x30);

    /* GPMC_WAIT0 */
    OUTREG32( g_CTL_base + CONTROL_CONF_GPMC_WAIT0,
                ( 0 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_MMODE_SHIFT) |
                ( 0 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_PUDEN_SHIFT)    |
                ( 1 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_PUTYPESEL_SHIFT)    |
                ( 1 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_RXACTIVE_SHIFT));

    /* GPMC_WPN */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_WPN,
                    ( 0 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_MMODE_SHIFT) |
                    ( 0 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_PUDEN_SHIFT) |
                    ( 1 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_PUTYPESEL_SHIFT) |
                    ( 0 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_RXACTIVE_SHIFT));

    /* GPMC_CS0 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_CSN(0), 0x00);

    /* GPMC_CS1 */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_CSN(1), 0x00);

    /* GPMC_ALE */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_ADVN_ALE, 0x00);

    /* GPMC_BE0N_CLE */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_BE0N_CLE,
                ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_MMODE_SHIFT ) |
                ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_PUDEN_SHIFT )    |
                ( 1 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_PUTYPESEL_SHIFT)    |
                ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_RXACTIVE_SHIFT));

    /* GPMC_OEN_REN */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_OEN_REN, 0x00);

    /* GPMC_WEN */
    OUTREG32(g_CTL_base + CONTROL_CONF_GPMC_WEN, 0x00);
}

void GPMCClkConfig(void)
{
    SETREG32(g_PRCM_base + CM_PER_L3S_CLKSTCTRL, CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    while((INREG32(g_PRCM_base + CM_PER_L3S_CLKSTCTRL) &
                                                CM_PER_L3S_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3S_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    SETREG32(g_PRCM_base + CM_PER_L3_CLKSTCTRL, CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    while((INREG32(g_PRCM_base + CM_PER_L3_CLKSTCTRL) &
                                               CM_PER_L3_CLKSTCTRL_CLKTRCTRL) != CM_PER_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    SETREG32(g_PRCM_base + CM_PER_L3_INSTR_CLKCTRL, CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE);

    while((INREG32(g_PRCM_base + CM_PER_L3_INSTR_CLKCTRL) &
                                              CM_PER_L3_INSTR_CLKCTRL_MODULEMODE) != CM_PER_L3_INSTR_CLKCTRL_MODULEMODE_ENABLE);

    SETREG32(g_PRCM_base + CM_PER_L3_CLKCTRL, CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE);

    while((INREG32(g_PRCM_base + CM_PER_L3_CLKCTRL) &

                                            CM_PER_L3_CLKCTRL_MODULEMODE) != CM_PER_L3_CLKCTRL_MODULEMODE_ENABLE);

    SETREG32(g_PRCM_base + CM_PER_OCPWP_L3_CLKSTCTRL, CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    while((INREG32(g_PRCM_base + CM_PER_OCPWP_L3_CLKSTCTRL) &

                                          CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL)  !=CM_PER_OCPWP_L3_CLKSTCTRL_CLKTRCTRL_SW_WKUP);

    SETREG32(g_PRCM_base + CM_PER_GPMC_CLKCTRL, CM_PER_GPMC_CLKCTRL_MODULEMODE_ENABLE);

    while((INREG32(g_PRCM_base + CM_PER_GPMC_CLKCTRL) &
                                         CM_PER_GPMC_CLKCTRL_MODULEMODE) != CM_PER_GPMC_CLKCTRL_MODULEMODE_ENABLE);

    SETREG32(g_PRCM_base + CM_PER_ELM_CLKCTRL, CM_PER_ELM_CLKCTRL_MODULEMODE_ENABLE);

    while((INREG32(g_PRCM_base + CM_PER_ELM_CLKCTRL) &
                                        CM_PER_ELM_CLKCTRL_MODULEMODE) != CM_PER_ELM_CLKCTRL_MODULEMODE_ENABLE);


    while(!(INREG32(g_PRCM_base + CM_PER_L3S_CLKSTCTRL) & CM_PER_L3S_CLKSTCTRL_CLKACTIVITY_L3S_GCLK));

    while(!(INREG32(g_PRCM_base + CM_PER_L3_CLKSTCTRL) & CM_PER_L3_CLKSTCTRL_CLKACTIVITY_L3_GCLK));
}

void GPMC_Init(void)
{
    //# Disable CS
    OUTREG32(g_GPMC_base + GPMC_CONFIG7(0), 0x00000000);
    OUTREG32(g_GPMC_base + GPMC_CONFIG7(1), 0x00000000);

    //WAITPINSELECT             Bit16
    //DeviceSize    16Bit =>     Bit12
    //MuxAddData                Bit9
    OUTREG32(g_GPMC_base + GPMC_CONFIG1(0), (1 << 16) + (1 << 12) + (1 << 9));
    OUTREG32(g_GPMC_base + GPMC_CONFIG1(1), (1 << 16) + (1 << 12) + (1 << 9));

    //CSONTME=0
    //CSWROFFTIME= 30 = 0x1E => Bit16
    //CSRDOFFTIME= 30 = 0x1E => Bit8
    OUTREG32(g_GPMC_base + GPMC_CONFIG2(0), (0x1E << 16) + (0x1E << 8));
    OUTREG32(g_GPMC_base + GPMC_CONFIG2(1), (0x1E << 16) + (0x1E << 8));

    //ADVONTIME = 4     = 0x04     => Bit0
    //ADVWROFFTIME = 10 = 0x0A     => Bit16
    //ADVRDOFFTIME = 10 = 0x0A  => Bit8
    OUTREG32(g_GPMC_base + GPMC_CONFIG3(0), (0x0A << 16) + (0x0A << 8) + (0x04 << 0));
    OUTREG32(g_GPMC_base + GPMC_CONFIG3(1), (0x0A << 16) + (0x0A << 8) + (0x04 << 0));

    //WEONTIME  = 14    = 0x0E    => Bit16
    //WEOFFTIME = 20    = 0x14    => Bit24
    //OEONTIME    = 14    = 0x0E    => Bit0
    //OEOFFTIME = 30    = 0x1E    => Bit8
    OUTREG32(g_GPMC_base + GPMC_CONFIG4(0), (0x14 << 24) + (0x0E << 16) + (0x1E << 8) + (0x0E << 0));
    OUTREG32(g_GPMC_base + GPMC_CONFIG4(1), (0x14 << 24) + (0x0E << 16) + (0x1E << 8) + (0x0E << 0));

    //RDCycleTime = 30    = 0x1E => Bit0
    //WRCycleTime = 30    = 0x1E => Bit8
    //RDACCESSTIME = 2  = 0x00 => Bit16
    //HWREG(0x50000070) = 0x000f1f1f;
    OUTREG32(g_GPMC_base + GPMC_CONFIG5(0), (0x01 << 16) + (0x1E << 8) + (0x1E << 0));
    OUTREG32(g_GPMC_base + GPMC_CONFIG5(1), (0x01 << 16) + (0x1E << 8) + (0x1E << 0));

    //WRACCESSTIME = 0      = 0x00    => Bit24
    //WRDATAONADMUXBUS = 10    = 0x0A  => Bit16
    //HWREG(0x50000074) = 0x000B0000;
    OUTREG32(g_GPMC_base + GPMC_CONFIG6(0), (0x00 << 24) + (0x0A << 16));
    OUTREG32(g_GPMC_base + GPMC_CONFIG6(1), (0x00 << 24) + (0x0A << 16));

    //HWREG(0x50000078) = 0x00000f41;
    //A24 = 1
    //start address = 0x01000000
    OUTREG32(g_GPMC_base + GPMC_CONFIG7(0), 0x00000F41);

    //A25 = 1
    //start address= 0x02000000
    OUTREG32(g_GPMC_base + GPMC_CONFIG7(1), 0x00000F42);
    
}