This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

pcie flow control

Hi

     I'm using the dm8168 as a root complex.The DM8168 and a FPGA are connected by a pcie(V2.0).As a master device,the DM8168 is writing a frame(1920*1080p60) of image data to FPGA through pcie.But,the rate of pcie is faster than 2.5Gbps ,and the FPGA processing speed is only 256Mbit clock.Half of one frame(1920*1080p60) of the image data will be lost by detecting.So,could i configure the pcie flow control in some register ?If i can,  and how can i get a freedback command from  FPGA in the protocal of the pcie.

thanks

                                                                              jianping   jiang