This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XDS510 PP(PLUS) emulator problem



Hi All,

I am facing a strange problem while connecting XDS510 PP emulator to C6727 DSP board.

Initially everything was fine and I was working with XDS510 PP emulator on my c6727 board. In between same Emulator started giving problem and not at all connecting to the same C6727 board, but working fine on DSK6713 board.

This is the error I am getting:

rror connecting to the target:
Error 0x80000200/-1073
Fatal Error during: OCS,
Bad Target Silicon Revision Number
Please check your multi-processor configuration.
The number of devices in the JTAG scan path
must be correct for the silicon revision to be read.
Or, you may have selected the wrong DSP device driver.


Sequence ID: 0
Error Code: -1073
Error Class: 0x80000200
I/O Port = 378

Board Name: C672x PP Emulator
Cpu Name: c672x

Abort:  Close Code Composer Studio.
Retry:  Try to connect to the target again.
Cancel:  Remain disconnected from the target
Diagnostic: Run diagnostic utility.

I did some R&D but could'nt find any solution to this problem, and even could'nt understand why its not working on some board. If there is some problem it should not work on any board?!!!  SDConfig diagnostic utility is also showing proper results.

The C6727board is perfectly alright, because I have tested with another PP emulator.

Please let me know if you have any solution to this problem.

 

Thanks,

Balachandra